Inquiry & Technical Confirmation: 200G QSFP56 DAC (NVIDIA MCP1650-V00AE30 Compatible)

------Question for MCP1650-V00AE30-C Please Put your question below------

Dear Sales Team,

I am writing to request a quote and technical confirmation for the ATGBICS DAC-QSFP56-200G-0.5M cable.

Before placing an order, we need to strictly verify the compatibility of this cable. We intend to use these cables for a dual-system interconnection between NVIDIA DGX Spark systems. Therefore, the cables must be 100% compatible with the NVIDIA/Mellanox MCP1650-V00AE30 specification.

Could you please confirm the following details?

  1. EEPROM Coding: Can you guarantee that the EEPROM on both ends of the cables will be specifically programmed to be recognized as MCP1650-V00AE30 by NVIDIA/Mellanox equipment?

  2. Pricing & Lead Time: Please provide a quote and the estimated lead time for [Insert Quantity] pieces of the 0.5m version.

  3. Return Policy: In the unlikely event that the cables fail to link up or are rejected by the DGX Spark systems due to coding issues, what is your return or replacement policy?

  4. Country of Origin: As per our procurement policy, we require products that are Non-MIC (Not Made in China) and preferably TAA Compliant. Please confirm the Country of Origin (COO) for these specific cables.

Thank you for your time and assistance. We look forward to your prompt response so we can proceed with the procurement process.

Best regards,

Shaun Lin Sales Manager Farsighttek 11F., No. 1, Sec. 4, Nanjing E. Rd., Songshan Dist., Taipei City 105609, Taiwan TEL: +886-955-296-828 FAX: +886-2-3393-0988 Tax ID: 42649177 Mail: sh


:taiwan: 中文版 (適合寄給台灣代理商或經銷商)

主旨:詢價與技術確認:200G QSFP56 DAC (相容 NVIDIA MCP1650-V00AE30)

業務團隊您好,

來信希望能針對 ATGBICS DAC-QSFP56-200G-0.5M 這款線材進行詢價與技術確認。

在正式下單前,我們需要嚴格確認此線材的相容性。我們預計將這些線材用於 NVIDIA DGX Spark 雙系統互連。因此,線材必須 100% 相容於 NVIDIA/Mellanox MCP1650-V00AE30 規格。

能否請您協助確認以下細節:

  1. EEPROM 寫碼: 貴司是否能保證線材兩端的 EEPROM 在出貨前,會特別燒錄為 NVIDIA/Mellanox 設備可完全識別的 MCP1650-V00AE30 編碼?

  2. 報價與交期: 請提供 [請填入數量] 條 0.5m 版本線材的報價與預估交期。

  3. 退換貨政策: 萬一線材因編碼問題無法連線,或被 DGX Spark 系統判定為不相容,貴司的退換貨政策為何?

  4. 原產地證明: 依據我們的專案採購規範,我們需要非中國製造(Non-MIC)且最好符合 TAA 規範的產品。請確認這批特定線材的原產地(COO)。

感謝您的協助,期待您的盡速回覆,以便我們推進後續採購流程。

順頌 商祺

林永樹 (Shaun) 業務經理 永視科技有限公司 105609 台北市松山區南京東路四段 1號11樓 TEL: 0955-296-828 FAX: 02-3393-0988 統編: 42649177 Mail: shaun@farsighttek.com Web: www.fars

您好 @shaun1

歡迎來到 DigiKey 技術論壇,感謝您的詢問。

根據您的具體需求,我認為技術論壇並非處理此諮詢的合適管道,因為其中涉及一些銷售政策方面的問題。

建議您使用英文向我們的 orders@digikey.com 工作人員發送電子郵件尋求協助。

謝謝 。