IP Rating

------Question for 8315100142 Please Put your question below------

Does this particular fan have the IP68 rating? Because the brochure states it as optional.

Hi @bohdan.burdash ,

Welcome to DigiKey TechForum and thanks for your inquiry.

No. This specific part number, 8315100142, does not have an IP68 rating.
Its standard protection rating is IP10.


Why the brochure says “IP68 – optional”

The AxiForce series brochure lists IP68 as an option because ebm‑papst offers factory variants (or configurable options) with enhanced sealing. However, IP rating is tied to the exact orderable part number, not the generic series name.

OK, so what is the correct part number for the equivalent IP68 rated fan ?

Hi @michael.filgate ,

Welcome to DigiKey TechForum and thanks for your inquiry.

The datasheet’s statement:

Degree of protection up to IP68

means that ebm‑papst can supply specially configured AxiForce variants with IP68 sealing, but the IP68 version has its own order code, and that order code is usually assigned through ebm‑papst sales/configuration (custom part number) rather than published as a generic replacement.

image

Would it be possible to purchase this custom configuration through DigiKey or does it have to be handled directly with ebm-papst?

Unfortunately, we don’t carry the custom part.
Please contact ebm-papst directly.
Thank you.

Hi

In terms of similar parts we can offer in stock, the following may be worth considering:

PFB1224HE-00P6 FAN 120X120X38MM, 24V, PWM, IP68, Locked Rotor Protection, PWM Control, Speed Sensor (Tach)