Is AO852A++ Hot Air Station suitable for use in Australia ie 24V 50Hz

Hi,
I’ve just ordered (O/N 93061484, 11th June 2025) an AO852A++ hot air station, but now I’m not sure if it is suitable for use in Australia. where we use 240 V and 50hz power. I ordered the same brand soldering station some years ago from you and it was fine, but I thought it best to check. The order is currently on hold.

Hello! Looks like this was solved over the phone, I’m the tech that spoke with you and our sales rep this morning.

For anyone else who might be looking into this, here is the breakdown.
2260-AO852A+±ND = 110VAC
2260-AO852A++220V-ND = 220VAC