------Question for MCT024L6W240320PML-1618BIT Please Put your question below------
I want a small display for my project. I see the MCT024L6W240320PML-1618BIT (https://www.digikey.in/en/products/detail/midas-displays/MCT024L6W240320PML-1618BIT/15630487) has controller type as ILI9341. Is this already included as part of the display package? If not how to add that separately? And what is the connector used to communicate with a microcontroller?
Welcome to the community!
The MCT024L6W240320PML-1618BIT already has ILI9341 integrated as part of the display assembly. The flat flex cable is a 40-position 0.5mm pitch that is 0.3mm thick. I narrowed the FFC type connector options down to the options here. Please double-check the drawings for the connector to make sure they will work in your application.