Is the RC522 Reader Module (CN0090) 5V-tolerant?

------Question for CN0090 Please Put your question below------

I’m looking at DigiKey Part # 4411-CN0090-ND and was wondering if it’s 5V tolerant, that is, can I use 5V on the VCC pin? Thanks for the help!

vincentchov, welcome to the TechForum! The datasheet and SunFounder’s part page both say “13-26mA/DC 3.3V.” This typically means it is supposed to be an exact value, so it seems like you wouldn’t be able to use 5V alone. You probably could adapt your setup so you can use a 5V source through a DC DC converter though.