ISM92-3351AH-50.000MHZ - Output status when oscillator is disabled

------Question for ISM92-3351AH-50.000MHZ Please Put your question below------

What is the behavior of the output pin when the oscillator is disabled? I need to provide 50MHz to a pin, but this pin share other I/O signals. If leaving this oscillator is disabled, would this mean Hi-Z state on the output pin? I cannot see any reference in the datasheet. Thank you.

Hello daniel.herrera and welcome to the DigiKey TechForum.

I couldn’t find any documentation related to this series, but I would assume the output levels would be what is shown as what 0 equals on the datasheet when this device is disabled. I do not see that it is listed as having a tristate pin, which they do state would cause a hi-z state, so I wouldn’t know for certain if it is put into a hi-z state, but I would assume that it is at least set to logic level 0.

1 Like