IT vs OT in Industrial Automation: Safety, Determinism, and Buffered Edge Architecture

There is a tension between IT and OT in industrial control systems. Ownership boundaries are defined in terms of machinery operation with priority given to safety and real-time deterministic requirements.

For clarity, we associate IT with vertical data transfer into the enterprise network. By contrast, OT is associated with machinery on the factory floor and machine to machine data transfer.

Key Takeaways

  • We have smart hardware that never gets updated (let’s be honest) behind our industrial firewalls. The seemingly secure vertical integration leaks into the horizontal.
  • Deterministic machine and process control are non-negotiable.
  • OT and IT teams live in a constant state of constructive tension.
  • OT interfaces with IT using clear descriptions of PLC buffers and protocols.

This article is part of the DigiKey Field Guide for Industrial Automation

Location: Teach It → Industry Context
Difficulty: :gear: Engineer — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 12 Oct 2026


Figure 1: Workbench image — populated with a safety PLC and safety-rated distributed I/O.

A Linux Host Hiding Behind Your Firewall

Let’s begin our IT vs OT discussion with a scar. Many years ago I worked in a lab that had an advanced GPS receiver connected to a flat network (a common broadcast domain). An outside port was opened for this GPS receiver, allowing timing data to be remotely retrieved. This was a terrible idea from a network security perspective as the GPS receiver contained a small Linux host. With an open port, the remote user could SSH into the GPS and then access the network. Using this technique, Eve and Mallory had internal network access from behind the firewall, as if they had just connected a local laptop to an open network port. That GPS receiver wasn’t a secure piece of hardware, it was an unpatched and unmonitored digital doorway into the network.

Network Classification at the Machine Interface

With regards to networks, we can classify machine control as:

  • Safe: This includes the safety PLCs, light curtains, E-Stops, and networks such as PROFISAFE. This is where we design for the Safety Integrity Level (SIL) or Performance Level (PL) requirements. Any network failure will cause the machine to enter a fail-safe state.

  • Deterministic: This category includes time-critical signals that a machine requires to operate. Ethernet-connected distributed remote I/O (not specifically identified as safety-rated). An example is a central PLC in a distribution center that coordinates the movement of objects on a conveyor. A network failure disables the machine but does not make it unsafe for the operator (when viewed through a SIL/PL lens).

  • Buffered Edge: This class of communication is important but not deterministic. This is where the horizontal factory floor interfaces with the vertical enterprise network. Staying with the conveyor example, the vertical computers provide “what goes where” data. The PLC provides telemetry data for the folks in the control room: job status, speed, rejection, and faults. The use of buffers differentiates between edge and deterministic control. The deterministic signals live close to the PLC scan cycle while edge devices are more tolerant of network fluctuations. A network fault is tolerated and even expected. However, this does not imply network communication is inconsequential as our example conveyor does not move without external instructions.

There is zero room for negotiation when it comes to safety systems. The design as well as the continued maintenance of this reflexive safety network falls squarely on the shoulders of the machine designers including the PLC programmer. This is OT territory. Each hazard must be identified and appropriate SIL/PL mitigation implemented.

The deterministic interface is generally a function of the OT team. This could be visualized as a set of “do upon network failure” settings for the distributed I/O.

In my opinion, the IT and OT edge boundary is best viewed as an agreement on the buffer mechanism (Figure 2). Together, the teams define handshake, retry, network glitch, as well as power-failure protocols. For example, the PLC may store critical messages in a retentive buffer while a larger buffer holds non-critical messages. This article presents a prototype for a PLC-side buffer. Here we can see the essential fields including running sequence number, head and tail pointers, status, and the message buffer itself.

Tech Tip: Version control can be a nightmare for maintenance. This is especially true when there are multiple smart devices on the network. The worst case is when the sensors, switches, and PLC all have different software. Here, technicians must be skilled in all environments and the “golden” configuration files for each device must be independently preserved.

There is a good argument for integrating all machine-programmable hardware into a single software development environment. Yes, this can be expensive, but that cost is amortized across every minute of saved downtime.

Figure 2: Priority ring buffer type definition.

Network Hygiene and Burden of Responsibility

Networks are complex. There is a chasm between just making things work and making things reliable under all conditions including graceful failure when things go wrong. Also, cybersecurity adds to the complexity.

Now consider preferences:

  • The IT instinct tends toward visibility and central control (policy) across the entire infrastructure. IT sees updates as routine.

  • The OT instinct is to lock things down with an emphasis on safety and deterministic communications. OT is deeply suspicious of anything that could potentially impact safety and determinism.

  • Let’s not forget the plant manager and the technicians that repair the machine. When things break, they want the ability to quickly restore the equipment. For example, a layer-3 Ethernet switch controlled from within an integrated software suite such as TIA Portal is easier to handle than a third-party switch.

Rather than point fingers about who is correct, let’s explore this from the burden of responsibility perspective. We have arrived at the edge of human limitations. Yes, in theory, a skilled PLC programmer and OT extraordinaire could claim the entire horizontal OT boundary. IT would be presented with a single semi-isolated port on the PLC. But what about that simple GPS receiver lurking on the network? Does the OT have the necessary skill set to identify and then mitigate all hazards.

Unlikely, and it would take decades to grow that skill set.

Likewise, IT is unlikely to have the skills required to understand the safety and deterministic timing of the PLC-based machinery.

Consequently, we arrive at the disquieting conclusion that OT and IT live in tension. It’s a productive tension that requires the best of both teams. OT preserves the machine’s autonomy via safety and crash-resistant determinism. The teams then work together at the interface level (e.g. buffers) to ensure reliable data transport, sound configuration of infrastructure, and best cybersecurity practices.

:books: Continue Exploring Industrial Control Systems

If this discussion was helpful, you may also want to explore:

:world_map: DigiKey Navigation

:japanese_symbol_for_beginner: Related Foundational Articles

About This Author

Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.

Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.

Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.

I am interested in opinion from the technical community here. It relates to the article to some extent. I have been a DigiKey customer longer than most.

For a couple of decades we have been supplying a controller for automation predominantly in markets where a PLC is not justified (e.g. Digital Cinema). Recently we have been looking to introduce the product generally in industrial controls markets. It has, through word-of-mouth, found applications there already but remains generally unknown. It is a well-supported tool and has even been handling MQTT since before Alexa was born.

I have discovered that this is considered an “edge” device. While it is a new term for us, it is also not well defined in my mind.

DigiKey has suggested (some time ago) that we are a candidate for Marketplace. It makes sense given that about 30% (dollar volume) of the JNIOR product cost comes from components purchased from DigiKey. We have just gotten lost in the procedure given that our product is not a commodity component available anywhere else. So no joy at this point. We haven’t gotten it done.

I am interested in any thoughts as to the “edge-icity” of our thing. It runs on Renesas RX MCUs and yet some would swear it is a Linux boot. But, it is not. We have a closed hardware and OS solution with all application programming being considered as open.

I developed all of the hardware since 2004 and wrote then entire OS (no 3rd party code at all). I can answer anything about it.

Thank you, @bscloutier,

Yes, your JNIOR and associated products are unquestionably in the “edge” category.

This image from the JNIOR 410 datasheet demonstrates the utility in an industrial setting. As I understand you have included robust hardware with optical isolation and relay outputs.

As for selling with Digikey, I would encourage you to reach out to DigiKey’s Marketplace team.

Sincerely,

Aaron

Aaron,

Does the term “edge controller” imply devices that provide network connectivity such as a full-featured web server with server side scripting (PHP-like in our case)? Does the ability to make data connections with the flexibility to program (Java managed language) protocols and handle protocol conversions, play into that designation?

Or does “edge controller” imply controls implemented on single board computers (SBCs) running main stream operating systems at GHz speeds? Those then have the above abilities by default.

There is the discussion regarding determinism and the impact of multi-tasking. The latter being required in providing edge features as I understand them. I assume that there is the potential for a similar controversy at the boundary between a purely hardware control and the PLC?

Does the “edge” device need to also be open? I have written a purpose-built OS from the ground up with the goal of providing bug-free fully-supported devices. It is closed in that we need to maintain control over it. That allows us to question even the slightest anomalous performance and then to definitively seek out the cause.Yet, the closed OS seems to be frowned upon by edge enthusiasts even though this OS is general purpose and all of the programming that runs on it we consider to be open.

Hello @bscloutier,

Allow me to explain using the SIMATIC IPC427E as an example. I would describe this as one bookend for the term “edge controller.” At the other end we find stand-alone devices advertised as “edge-connected” systems.

What I’m trying to say is that “edge” does not appear to have a single meaning. As implied in the article, the term is associated with IT entering OT territory.

IMO, there is no correlation between “edge” and “open.”

The marketing questions are outside my wheelhouse. There are certainly strong opinions for and against open and closed.

Let me leave you with one thought: equipment availability is the 2nd most important consideration for industrial settings immediately following safety. If the line isn’t running the company is out hundreds to tens of thousands of dollar per minute. This reality tends to dominate all other consideration.

Sincerely,

Aaron

Interesting. I hear this as well from someone here who used to work at an Intel fab (with loss rates much much more staggering). Thank you for reinforcing that. It may be obvious but…

This is why we have avoided the involvement of 3rd parties in firmware. If I am to be responsible for reliability and stability, not to mention function, I need to be in a position to immediately address anything that comes along. There cannot be anywhere to point fingers. No bug lists and schedules to get on. We even do our own production so as to be in control of product availability. I am so obsessive DIY that I have even threatened to fab our own ICs. Joking of course. But when I hired someone who just happened to come out of Intel, some eyebrows got raised.

I suppose SBC Linux boot controls do have to contend with updates. I can’t say that I have ever used a computer that hasn’t locked-up, required reboots or received a problematic update. My pick and place run Windows. So we air gap those.

Yes, @bscloutier.

This is where the fun begins. It’s one thing to make it work but another thing entirely to make it work for days, months, or years.

For some light reading, I encourage our readers to look into MISRA and related code standards. I find it humbling as there are so many things I do not know.

Sincerely,

APDahlen