Jauch CR1620 Discharge rate

------Question for CR1620 Please Put your question below------

The specifications for the 1908-CR1620JAUCHSB-ND indicate the discharge rate for this model is 650µA, which seems quite a bit higher than comparable models. Is this correct or possibly a typo?

Add adding to this, I assume the discharge rate is what the battery can provide when a load is connected and drawing.

Hello,

Welcome to the TechForum.

Yes, the 650µA matches the .65mA ratings for discharge so this looks accurate from the datasheet.

Thank you
Ryan

1 Like

Oops, I forgot to cross-check with specification sheet - thanks for linking that. I was comparing the Jauch CR1620 to the Murata CR1620. The Murata’s specification sheet appears to be a dead-link. Do you have a copy of it or can you obtain a new link to its specification sheet?

Hello @bigdummy,
This part is being transferred from Murata to another manufacturer. This will be made by Maxell here is their Datasheet

You can see Murata’s notice Click Here

1 Like

@Troy_2808, thank you. From their spec sheet, Murata/Maxell have collected discharge data at over 1000µA. I’ll give those a try!

1 Like