JST Connector - Missing

Hello I have a WhisperKool wine condenser that is is being installed. The thermostat wire was not properly protected and the JST connector is now missing that would connect the wire to the thermostat. Can I just purchase a new plastic connector and attach the three wires (could the solution be that simple?) or do I have to replace and fish a new thermostat wire?



The later pictures are the connector at the other end of the wire that are intact.

Hello n_walz,

The wiring does not appear that it is damaged on the image provided. It is possible that you may need to replace the contact as well as the housing, as the part of the contact that holds it in the housing may be damaged/bent so that it would not stay in the housing.

I did look to see if I could find a JST connector as a replacement but unfortunately, couldn’t be certain if we carry the particular one you are wanting to replace. If you are able to provide more information in regard to what you are trying to replace, we may be able to locate something for you.