# LD4A05P0

**URL:** <https://forum.digikey.com/t/ld4a05p0/14181>\
**Category:** Industrial Automation and Control\
**Tags:** automation-and-control, red-lion-controls, terminology, industrial-automation-and-controls\
**Created:** [May 12, 2021, 1:48pm UTC](https://forum.digikey.com/t/ld4a05p0/14181 "2021-05-12T13:48:44Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![KefanZhou](https://avatars.discourse-cdn.com/v4/letter/k/9de053/32.png) [@KefanZhou](https://forum.digikey.com/u/KefanZhou)\
**Post date:** [May 12, 2021, 1:48pm UTC](https://forum.digikey.com/t/ld4a05p0/14181/1 "2021-05-12T13:48:44Z")

</div>

Hi,  
I would like to confirm following items for LD4A05P0 product:

1. If the input signal is 4-20mA analog, I will need to follow the following wiring diagram and need extra power supply.  
 ![image](https://global.discourse-cdn.com/digikey/original/3X/e/e/eeb94f58d3ee4e56866c7a40d099225ab118c699.png)

I am just confused about the word EXCITATION and CURRENT.  
Regards,  
KZ

---

<div class="post-metadata">

**Author:** ![rick\_1976](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/rick_1976/32/1571_2.png) [@rick\_1976](https://forum.digikey.com/u/rick_1976)\
**Post date:** [May 12, 2021, 3:29pm UTC](https://forum.digikey.com/t/ld4a05p0/14181/2 "2021-05-12T15:29:52Z")

</div>

If I read correctly, that refers to the case where the LD4xxxx is supplying voltage to some sensor that allows between 4 and 20 mA to pass in response to the quantity being measured. The EXC pin in that event would appear to be the one that’s supplying voltage/sourcing current, and the CURRENT pin the one that’s measuring how much current the sensor is allowing to pass.

---

<div class="post-metadata">

**Author:** ![KefanZhou](https://avatars.discourse-cdn.com/v4/letter/k/9de053/32.png) [@KefanZhou](https://forum.digikey.com/u/KefanZhou)\
**Post date:** [May 12, 2021, 3:43pm UTC](https://forum.digikey.com/t/ld4a05p0/14181/3 "2021-05-12T15:43:18Z")

</div>

Hi Rick,  
So if the transmitter is loop powered then the I would connect pin 4 and pin 3?

 ![image](https://global.discourse-cdn.com/digikey/original/3X/9/d/9df7f737a03b454025ae703488c746bb6b402306.png)

The transmitter I plan to use is not loop powered, so I think I should use pin 3 and pin 2?  
Regards,  
KZ

---

<div class="post-metadata">

**Author:** ![rick\_1976](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/rick_1976/32/1571_2.png) [@rick\_1976](https://forum.digikey.com/u/rick_1976)\
**Post date:** [May 12, 2021, 4:28pm UTC](https://forum.digikey.com/t/ld4a05p0/14181/4 "2021-05-12T16:28:16Z")

</div>

A 4~20mA transmitter that isn’t powered _by the loop_ does not necessarily _power the loop_. Many will simply provide what amounts to a variable resistance to modulate current flow through a loop that’s being driven by an external voltage source. Use 3+4 in such a case. If the device transmitting data also provides the voltage source necessary to cause current flow in the loop, use 2+3.

---

<div class="post-metadata">

**Author:** ![Kristof\_2649](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/kristof_2649/32/2325_2.png) [@Kristof\_2649](https://forum.digikey.com/u/Kristof_2649)\
**Post date:** [May 12, 2021, 5:23pm UTC](https://forum.digikey.com/t/ld4a05p0/14181/5 "2021-05-12T17:23:55Z")

</div>

Kindly see below diagram for function of Pin 4, EXC

 ![image](https://global.discourse-cdn.com/digikey/original/3X/2/6/268952fb6313f9ebe43cb8c6ed79b14fd4e1266f.png)

It is a source for 24VDC supply voltage for the sensor.

It would be used with sensors that can accept a 24VDC supply voltage with a current output signal.