I have a question about a specific item; I am looking for the BXRE-30G2000-B-833H LED COB.
When I enter this into DigiKey, the item 976-BXRE-30G2000-C-83-ND comes up as being in stock.
What is the difference, and can I use this as a replacement for the BXRE-30G2000-B-833H?
Hi info.vanonno,
Welcome to the TechForum.
According to the datasheet for the product line, the difference between the “B” and “C” versions are the current drive level they are optimized for.
The “C” version can be driven to higher current levels, resulting in higher brightness, though there is a broad overlap in drive current ranges, with the “B” version recommended min and max between 175mA and 1250mA while the “C” version min and max between 250mA and 1750mA.
From page 7 of datasheet:
Thanks for your answer, I eventually asked AI as well, and he said exactly the same thing. He asked about the brand and type of driver I was going to use and that was fine too; he even knew which settings were required, and I have already ordered the Cob Lets.
Kind regards, Onno