Let’s Talk Technical with Qorvo- QSPICE - Advancing RF Circuit Simulation

Topic Questions

What simulations are important for RF design?

  • Historically, RF designers avoided SPICE, preferring idealized linear, frequency-domain, or limited harmonic simulations, largely because traditional SPICE tools did not handle harmonic generation well. QSPICE addresses this by using time-step methods that enable accurate simulation of low-level nonlinearities - capabilities that until about five years ago were primarily the domain of harmonic balance solvers. The key message for RF designers is to do more work in the time domain, which offers significant advantages: it preserves the true physical bias point, captures full circuit nonlinearity, provides real power dissipation, and verifies the actual circuit without frequency-domain simplifying assumptions. While RF design traditionally emphasizes frequency-domain behavior, QSPICE derives this accurately from first principles by linearizing the real circuit at its actual bias point. Re-linearizing at each simulation run creates a more robust, lower-error design flow because it always analyzes the unmodified, literal circuit - and QSPICE excels at this.

What are the benefits of simulating RF designs?

  • Simulating RF circuits serves the same fundamental purpose as simulating any circuit. It builds understanding and intuition about how the circuit works. Simulation is especially valuable compared to bench experimentation because modern printed circuit boards are complex and multilayered, making components and routing difficult or impossible to modify. In simulation, however, designers can easily explore and understand circuit behavior in ways that aren’t practical on hardware. For RF design specifically, simulation allows PCB parasitics to be selectively removed or added, revealing how the core circuit behaves and which parasitics actually matter—something that cannot be done on a physical board. This ability makes simulation a uniquely powerful tool for understanding RF circuits.

What are some challenges in simulating high-frequency phenomena?

  • The main challenge in RF simulation is accurately identifying parasitics, since their true values are often uncertain. While simple analytical formulas - such as wire inductance equations - can provide useful approximations, and tools like QSPICE conveniently automate these calculations based on physical dimensions for structures like solenoids, striplines, and straight wires, it still takes experience to know which parasitics to model and how. A further difficulty arises when lumped constants are no longer adequate, as parasitic values can be frequency-dependent due to dielectric dispersion or magnetic material behavior at the atomic level. Because dispersion makes it difficult or even impossible to create accurate broadband lumped models, RF design flows must be robust and defensive against uncertainty in parasitic effects.

What are some things that were modified to ease the user experience in QSPICE?

  • Electronic engineering CAD tools have historically lagged behind modern user interface design. QSPICE addresses this by minimizing modal dialogs and unnecessary eye and mouse movement. Instead of opening separate forms to edit components - forcing users to shift focus away from the schematic - QSPICE enables in-place editing by double-clicking text directly in the schematic, even when that text is rotated or mirrored. This required specialized editors but results in a more ergonomic workflow. Additionally, QSPICE prioritizes context-sensitive right-click menus over toolbar buttons, reducing mouse travel and making relevant commands immediately accessible. Because only a small number of actions are meaningful for any given object or state, QSPICE uses concise, context-aware menus that are always available, resulting in a more modern and efficient interface than traditional electronic CAD tools.

YouTube Video Sources

If you would like to watch this video or any other Let’s Talk Technical Series, please utilize the sources below.

Video on this Topic

Let’s Talk Technical with Qorvo- QSPICE - Advancing RF Circuit Simulation | DigiKey

Other Videos from this Series

Let’s Talk Technical Playlist - YouTube

Supplier Featured in Video

Qorvo

image

Qorvo (Nasdaq:QRVO) supplies innovative semiconductor solutions that make a better world possible. They combine product and technology leadership, systems-level expertise and global manufacturing scale to quickly solve customers’ most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including automotive, consumer, defense & aerospace, industrial & enterprise, infrastructure, and mobile.