Looking for a transfo replacement

Hi Everyone! i am looking for a transfo replacement for a Leica battery charger. The Leica Battery charger model is GKL221.
The original transfo is 35.5MM wide and 35.5MM long
It has 13 pins
Thanks !

Hello antoine,

I wasn’t able to find anything in regard to the electrical specifications for this transformer. I did review the charger itself and tried to find something based on the information on its user manual, but was not able to find anything we carry that appears as if it would work. Do you happen to know the required electrical specifications for this transformer, such as primary and secondary voltage?

Hello Nick,
Thanks for the fast answer. The only informations i have is whats written behind the charger. INPUT : 100-240V 50/60HZ 1000mA/75VA
24V /2.5AMAX
OUTPUT 18.0V/4.0A MAX

I can read EDT-29 on the transfo. Thats all the info a have

Antoine

Sorry, @antoine,

High frequency power transformers such as this are notoriously difficult to source. They are often custom designed for the unit. Also, the replacement must be exact, or the unit will not function.

Recommend you purchase a replacement power supply. We may be able to select a replacement if the unit has a standard connector. Here are a few options.

Best wishes,

APDahlen

1 Like

Thanks for this useful answer. I’ll try to find a donor board. have a nice day
Antoine

1 Like