Hello,
I am looking for an adapter for the Metrohm 809 Titrando with the Ca-electrode. I need an adapter that fits these two sides (see attached images). After searching, I believe it BNC (female) to F-LEMO (Metrohm). That would be great if DigiKey has it.
Thank you!
Hello hg3nguye,
Welcome to the DigiKey TechForum.
I seached for an adapter, with a BNC with a female center socket on one end, and a LEMO connector with a male center pin on the other end.
The options I found are part numbers 1124-1001-ND and 1124-1304-ND.
To compare to your connector, the mating connectors for the LEMO end are 1124-1359-ND and 1124-1360-ND.
The differences in the manufacture part numbers for both pairs are an N or C. The N is for Nickel plating, and the C is for Chrome plating. So these are the same adapter/connector, but with a different plating option.
Hi David,
Thanks for advising. So both the 1124-1001-ND and 1124-1304-ND fit right?
hg3nguye,
Those are the ones I found when searching for an adapter, with a BNC with a female center socket on one end, and a LEMO connector with a male center pin on the other end.
You will have to check the datasheets to verify compatibility to your application.