Looking for correct pushbutton switch NO

Hello,

I am looking for a correct pushbutton switch that fits in our product. Preferable screw terminals connection, but soldering is also ok. The Push-button must be NO, spring-return. The button must be fixed through M16 gland hole, so 14,8mm inner diameter. The thickness of the housing is 6mm.

In picture you see a pushbutton NC rafi 1.1.0001 and fits. But this cannot be found online. Anyway this is a NC contact, must be NO. In other picture the TRU COMPONENTS 701283 shaft does not fit in hole

Can you help finding?

Hello @mzoon and welcome to the TechForum!

Please review this button 1715-1.10.001.001/0301-ND. Datasheet can be found HERE.

Best regards!

Hello mzoon,

If you are looking for pushbutton switches with M16 threads, Click Here for the available options. These all have the M16x1.0 threads, are SPST-NO, with screw terminals.

thank you David, but the M16 gland hole has screw size M16x1,5, so it will not fitt.
but you gave me an idea. i will search for APEM IA serie from Reichelt or Schlegel Rondit or Format serie

this Rafi button is round 15,2mm. i can only handle max 14,8mm or exact M16x1,5mm

i am coming out to Schlegel RRJVA_01 and Schlegel SVVA_01 Shortron series and Langir L16-M series . but still it is hard looking for the correct one

can you still help me with this?

Hello @mzoon

The closest options I see for a hole size near 14.8mm which are these options that fit hole size around 13mm. Please see link here

thank you, that can fit in the hole. but now the switch must fit in a 6mm housing. a lot of switches does not have a lot of length. also the collar must be min 17mm. search continues

Can you define what you mean by “the collar”?

I believe switches such as those form the C&K “AP” series would fit into your 14.8mm hole and would have sufficient length to fit a nut on the rear side of your panel.

Example:

The datasheet for the AP series does not give the actual depth of the threaded section, but I estimate it to be about 9.0mm, based on other dimensions given within the datasheet.

For scale, they do give the thickness of the nut to be 2.4mm.

thank you David. for disapearing the nut into the m16 hole inside, a ```
fender washer is needed. this is mostly 2mm thick. this causes that the nut fixing becomes 9-6-2mm= 1mm. so this is also not wanted.

pushbutton

thats why, i decided to stop searching and do it this way. drill hole in blind cable gland, put button through hole and thats it

we can close the ticket

OK, sounds good. Hopefully that will work for you. Sorry we didn’t have a nice simple solution to offer.

Thanks for contacting the TechForum, and best of luck to you!