Looking for model number or part. Power jack ANPCOWER labtop B02

Looking for Power jack to replace on a ANPCOWER model B02 labtop. Not sure if this is the correct forum location

@htcs

Would you have the dimensions for either the plug or the jack?

@htcs

Would need the inner diameter and outer diameter of the plug or the pin diameter and outer diameter of the jack.

outer diameter 6 mm wide 5mm high
the inside part was 4mm x 4mm

Do you mean the inner diameter of the barrel was 5mm, and the outer diameter was 6mm? The diameter should just be a single measurement across the tip of the barrel so noting it in “width by height” isn’t something we can use.

the inner diameter of the barrel was 4mm

To have a chance to find something, we need Inner Diameter (ID) of hole in plug barrel and Outer Diameter (OD) of plug barrel, as indicated in this diagram:

This came from the manufacturer today. So i am looking. thanks

  • Outer Diameter (OD): Typically 5.5mm.

  • Inner Diameter (ID): Typically 2.5mm or 2.1mm.

  • Polarity: Most importantly, you must confirm the polarity. For this model, it is most commonly center-positive, meaning the inner pin is positive (+) and the outer sleeve is negative (-). However, you must verify this on the original charger or board to avoid damage.

htcs,

That information helps, and 5.5mm is pretty standard. However, you will need to measure the original center pin, to verify if it’s a 2.1mm or 2.5mm diameter, that you need.

If you get the wrong one, it will either not plug in, or it will not make a secure connection.

The polarity would only be important, if you were replacing the power supply.