Hi, I am looking for this contact socket power. Please help me.
Hello @bryan.degamo
Thanks for posting! Could you share the overall dimensions of that contact (length, width, and height)?
A photo from another angle would also help.
Thanks!
Hi Jon_11475,
Please see the attached Excel file for the connector dimensions.
Thanks,
(attachments)
Connector Dimension.xlsx (337 KB)
Hello @bryan.degamo,
Thanks for the dimensions and extra photos! It looks similar to the dual-blade power contacts used inside headers like Samtec’s PowerStrip PET series, for example PET-06-02-L-VT (DigiKey PET-06-02-L-VT-ND)
Unfortunately, I couldn’t find simliar contacts in our catalog offered on their own, without the header housing.
Hello @bryan.degamo,
I apologize. I was focused just looking for the contact.
With the housing on, this looks like a Molex Mini-Fit Sr. 6-position vertical header. The contacts aren’t sold separately, so the replacement would be the full header:
Molex 0428196244 (DigiKey 0428196244-ND) per your 7.56mm measurement.
Drawing linked HERE.
If you also need the mating cable side, the matching receptacle housing is Molex 0428160612 (DigiKey WM1931-ND). Its crimp contacts are sold separately; scroll down to the Associated Products section on that page to find them.
Hi Jon,
This is exactly what I’m looking for. We will purchase this.
Thank you so much.
regards,
Hello @bryan.degamo, thank you for your question.
From your photo, this looks like a ceramic capacitor rather than tantalum, since it has no marking or polarity stripe. I was unable to locate a capacitor with those specific requirements (80 uF, 15 V, 20%), but you can search our ceramic and tantalum capacitor categories here:
Ceramic Capacitors
Tantalum Capacitors
To narrow the results, use the filters at the top of the page:
- Capacitance: select the closest uF value.
- Voltage - Rated: select 15 V or higher.
- Tolerance: select ±20%.
- Mounting Type: select the Surface Mount options.
- Package / Case: select the size that matches your part (measure its length and width).
- Check In Stock, then click Apply All.
The closest value we have in conformally coated tantalum capacitors is 80uF. We jump from 68uF to 100uF.