LTE Cat 1 module with built-in eUICC that can download consumer (SGP.22) eSIM profiles?

Hello,

We build an e-bike telematics unit (ESP32 + LTE module) in Nepal. Our local operator gives IoT SIMs only as a consumer eSIM with a QR code (SGP.22, SM-DP+ address + activation code). Our current modems (SIMCom SIM7600E, Quectel EC20) have no eSIM inside, so they cannot use it.

We are looking for:

  1. An LTE module with a built-in eUICC that can download and enable an SGP.22 profile from a QR code / activation code, using AT commands (no phone, no app).
    • Bands: LTE B3, B8, B20, plus 2G 900/1800 fallback
    • LTE Cat 1 is enough
    • The eUICC must be open (not locked to one IoT platform)
  2. Or: a module that supports AT+CCHO / AT+CGLA / AT+CCHC or AT+CSIM, so we can use an external eUICC chip with an open-source LPA (lpac).
  3. Blank SGP.22 eUICC chips in MFF2 (soldered) package, if DigiKey sells them.

Questions:

  • Which part numbers fit, and are they in stock at DigiKey (1-10 samples)?
  • Is the eUICC open, or locked to one provider?
  • Is there an app note with the AT commands for profile download?

Thank you,
Sandesh Bhusal
Evon Electric Pvt. Ltd., Nepal