Indirect array addressing is a rite of passage for the PLC programmer, as it unlocks higher-level programming such as storing and retrieving large amounts of data. Playing a song is a classic way to learn arrays and indirect memory access. This article presents a PLC implementation allowing the Pulse Train Output on a Siemens S7-1200 PLC to sing through a speaker.
This article is part of the DigiKey Field Guide for Industrial Automation
Location: Program It → PLC → Siemens S7-1200 and S7-1500
Difficulty:
Student — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 06 Mar 2026
Introduction to Indirect Addressing in PLC Arrays
An array is an ordered grouping of memory elements where all elements have the same type. In the Programmable Logic Controller (PLC), we define an array by declaring the memory type as well as the size of the array. For instance, we could construct a single-dimension array to hold the barcode information as containers move on a conveyor. In this application, the first barcode would be stored as barCodes[0].
What is indirect addressing?
Array elements may be accessed using direct or indirect methods:
-
Direct: A constant is used to identify the array element of interest e.g.,
barCodes[1]. -
Indirect: A variable is used to identify the element of interest e.g.,
barCodes[x]wherexis an unsigned integer bounded by the size of the array.
Indirect memory access is an inseparable tool when working with arrays. It allows the programmer to iterate over an array. In the previous example, we could declare an unsigned integer containerCount. We then access the array elements as barCodes[containerCount]. As each container passes, we increment containerCount and then store the barcode.
Indirect addressing is a rite of passage for any programmer. It’s a challenging concept. However, once mastered it opens many possibilities. Our opening barcode is a good example. Another is the ability to capture and store error messages for display on an HMI. With arrays, the technician could scroll through the error messages to determine the root cause of the error.
Indirect Addressing Demonstrated by Playing a Song
Playing a song is a classic method used to teach indirect addressing to embedded microcontroller programmers. Arrays are used to hold the musical notes, while a timer is used to advance to the next note.
This same technique can be used for Siemens TIA Portal and the S7-1200 as pictured in Figure 1. While the PLC isn’t typically considered a music box, it does have multiple pulse generators, typically used to drive motors. These generators may be repurposed to drive a speaker, providing music with a 1980’s video game vibe.
To make the PLC sing, we configure the pulse train hardware. The result is included in Video 1 where the PLC plays Scott Joplin’s “The Entertainer” piano rag.
Figure 1: The Siemens S7-1200 PLC is mounted on a Phase Dock trainer.
The Joplin song shown in Video 1 moves fast and contains over 100 notes (including the musical rests). As a lifetime musician, it was easy to identify the notes from the sheet music. The hard part is correctly (manually) converting each note into a frequency. Perhaps I should have written a computer program, but instead I used a spreadsheet.
Video 1: The Siemens S7-1200 “singing” Joplin’s “The Entertainer.”
How to Initialize Array Elements
My technique is described in this article. There you will find a description of the Siemens Data Block (DB) along with the intermediate spreadsheet used to initialize the array elements.
Tech Tip: The Siemens Data Block (DB) provides a portable memory container. This DB object is the native Siemens way to handle memory. As shown in a previous article, combining the DB with a spreadsheet or computer program provides a convenient way to transfer data into the PLC.
How to Control the Siemens Pulse Generators (PTO and PWM)
The Siemens S7-1200 includes pulse generators that can be configured for Pulse Train Output (PTO) or Pulse Width Modulation (PWM). In this application, we use the PTO as it allows dynamic frequency adjustment while maintaining a 50% duty cycle. The instantiation is shown in Figure 2. There we observe the indirect addressing of musicalNotesDatBlock.note[#uiIndex]. Note that uiIndex is a pointer to the next note while a rising edge on xLoadNote will transfer the note to the PTO block.
Please refer to this link for instructions to configure the Siemens PTO.
The code for the music UDFB may be downloaded in pdf form. It’s a relatively straightforward approach to generate a pulse every timNote seconds. This pulse is used to increment uiIndex and to load a new value in the PTO block. Finally, a guard is used to reset uiIndex at the end of the song.
playSong.pdf (75.7 KB)
MusicalNotesDataBlock.db (3.2 KB)
Figure 2: Instantiation of the Siemens PTO hardware to play the musical notes.
Speaker connection
A small speaker was used as shown in Video 1. A series current resistor is used to both protect both the PLC’s solid-state output and the speaker. As a starting point, use a 1 kΩ resistor and adjust as necessary to control the volume.
Next Steps
This article provides a working example of indirect array addressing. You are encouraged to experiment:
- Change the song
- Use a multidimensional array to hold both note and duration.
- Instantiate another PTO to play a countermelody
- Use the indirect addressing technique to construct a lookup table simulating the operation of an industrial clothes washer
- Construct a Simon Says game using indirect addressing to play the moves and track the player’s response
- Use arrays to record robot arm positions for playback.
Parting Thoughts
PLC programming concepts don’t need to be abstract. Programming music is a very good exercise that sets the stage for future learning. Your students will have a solid understanding of arrays, and they will be ready to step to motor drives (excuse the pun).
Please give this technique a try and share your observations in the comments section.
Best wishes,
APDahlen
Continue Exploring Industrial Control Systems
If this discussion was helpful, you may also want to explore:
DigiKey Navigation
- Full Catalog: Industrial Control & Automation
Related Foundational Articles
- Building a State Machine in Siemens TIA Portal
- Maximize Variable Frequency Drive (VFD) Lifetime with Proper Link Capacitor Care
- Relay Logic for Industrial Control Panels Part 1
About This Author
Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.
Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.
Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.