MID TERM LOGGING (7-8 DAYS) CAPABILITY

Hi,

The specification mentioned that the battery life is 10 hours, and memory up to 2000 lines. But we need to do minimum measurement duration of 8 days, at 30 minutes interval. Can you please confirm if this is doable, within the existing system you’ll supply. Or, if we need to connect to external memory (if say, we want to reduce the interval to 15 minutes, where the memory of 2000 lines might not be sufficient?) or connect to continuous power supply for continuous battery charging to support more than 10 hours logging? Appreciate your feedback. You can also contact me at REDACTED, Aziz. Thank You.

You will need to provide a part number for your question.

1 Like

FDT25 (PORTABLE DIGITAL ULTRASONIC FLOW METER KIT - OMEGA)

The manual shows that the FDT-25W is to be powered with either 220VAC or 24VDC. The battery looks to be there as a backup during power loss.

Hi thank you for your reply. What about 2000 lines memory. For 8 days, at 15 minutes interval, can this memory support the data within existing meter’s internal memory?

regards,

I don’t in the manual were it is stated that there are 2000 lines of memory.

There is a note in the other functions that it automatically records the time of power-on/off and the flow rate of the last 30 times.

image

The operation of this unit is send the output using one of the connections noted below. Using it as a stand alone datalogger looks to be outside of the intended purpose of this unit.