MOLEX 1301410056

Hello Team,

Please help to share the material drawing of MOLEX 1301410056. We need to confirm its mechanical dimensions. Thanks!

Hello shann.npd1,

This part doesn’t seem to have a drawing associated with it and as per Molex, only the data sheet is available here:

Wiring Devices Part 1301410056 | Molex

Hi @Irfan_Koric,

Thank you for checking on this.

Since no drawings are available, how can we accurately assess the actual dimensions?

It seems it would be the standard NEMA L5-15 but I’m checking with the manufacturer to see if they can provide the drawing for it. I’ll update you with whatever they come back with.

Hi again shann.npd1,

I’m sorry to inform but our contacts at Molex informed that there is no drawing for this item.

Sorry for the inconvenience.

Hi shann.npd1,

Typically, customers are not concerned with precise dimensions of a plug designed to be attached to the end of an outdoor extension cable since it does not have to fit into a carefully defined space. This is probably why the dimensions seem difficult to find.

However, I did find the dimensions specified below for the Molex 1301410056 (Molex owns the Woodhead brand) at this website.

Cord Diameter: 0.335 to 0.64 in
Dimensions: 1.66 in Dia x 2.99 in L

I have no way to verify that these dimensions are correct, but based on the image and the known dimensions of the NEMA L5-15R socket contact diameter (about 0.7"~0.8"), it seems about right.