Molex Connector

Does Molex offer the following connectors 1210230122 ; 1210230242 ; 1210640087 ; 1210640918 as a single part number that includes a PG09 8mm cable grip gland (similar to Phoenix # 1424496 4-8mm cable grip gland)? Currently I’m purchasing the connectors and cable grip glands separately and swapping out the cable grips that come with the above-mentioned connectors.

Hello djdemsic, welcome to the TechForum,

The only thing we would have with a cable gland is in this link: Sensor Cable Accessories | Sensors, Transducers | DigiKey

Hi djdemsic,

The valve connectors in this link use an external thread type of cable gland rather than an internal thread type of gland like the Phoenix # 1424496, but they can handle cable from 4.00-9.00mm.

Example image:

On the remote chance that you could use valve connectors with pre-assembled cable, here’s a link to some options for that as well.

From my experience, those connectors are modular assemblies.The cable gland is usually ordered separately. I have not seen a combined part number.
Molex often lets users choose cable gland sizes.

That provides flexibility for different cable diameters.