Hi, I’m currently trying to identify this Female Socket Terminal. I believe it is a Molex terminal, the 1381 series is similar in design although it is too large. Molex Series 150181 is a similar length but is not the right diameter. The OD is 2.8mm, and the length is 16.7mm
Thank you for your inquiry and welcome to the community.
We do not have ability to search for contacts based on measurements.
To be able to assist in identifying associated contacts, it would be of great help if you could kindly provide a picture of the connector housing these contacts are used with, and also a measurement of the spacing between one contact to the next, what we call ‘pitch’ of the connector.
Provide a diameter dimension of the mating pin. That might help too.
The mating pin is 2.3mm in diameter
Hello @waterwise,
I’m stumped.
Maybe the socket contact was stretched out to accommodate the pin? The part looks so common (TE or Molex), but the dimensions don’t line up with anything I could find. It’s possibly a generic contact.