Motor Fan Efficiency

------Question for MF35100V1-1000U-G99 Please Put your question below------

I would like to know the efficiency of the Motor Fan with the model number MF35100V1-1000U-G99. Thank you very much.

Sincerely

Hasan Rouf

Hello! The manufacturer doesn’t have a specific efficiency or FEG rating listed for this part. They have a pressure vs CFM chart on page 5 of the datasheet for reference.

Doing some rough math with the nominal values gives us Static Efficiency = ~27.38%. However, this isn’t the same as the total or maximum efficiency, as it will depend very much on the conditions it is being run or tested in. Hopefully one of our engineers will we able to provide a little more guidance, that’s about as much as I know on the subject, my math may be off on this one.

Greetings,

It would be necessary to define more precisely what is meant by “efficiency” in order to respond to such a question, because (among other things) the answer is likely to change depending on the selected operating point.

Because of the complexity involved in doing so, it is rare to find such information made available in the context of small fans of this type. A more common practice is to select candidate devices based on other more easily defined criteria, and evaluate them under the intended operating conditions for other characteristics such as power consumption.