Motor Switch

------Question for 3120-N521-H7T1-W01D-12A Please Put your question below------

I have a broken Weber Unimat WT22-55-551 15A 4 pin switch.

Will the suggested replacement meet my requirements.?

We have a number of similar switches, linked here: DPST Rocker Switches

But to be more certain of a replacement we’ll need to know the dimensions of the panel cutout, it would help if you had a description or clear photo of the switch showing the part markings as well.

IMG_20260317_0002.pdf (767.6 KB)

Panel Cutout 44mm x 22mm

44MM BY 22MM Panel cutout

Okay, based on that measurement it seems like our only option available is part number 432-1274-ND.

We only list the DC rating but I checked the manufacturer’s datasheet and it does clarify that the contacts are rated for 15A at 125VAC.

This is not a direct cross-reference item, so take a look at the specs and make sure it meets your requirements. Hope this helps!