# NanoEdgeAIStudio: An Automated Machine Learning Tool for STM32 Developers

**URL:** <https://forum.digikey.com/t/nanoedgeaistudio-an-automated-machine-learning-tool-for-stm32-developers/42631>\
**Category:** Development Boards, Kits, Programmers\
**Tags:** stmicroelectronics, evaluation-boards\
**Created:** [June 27, 2024, 7:10am UTC](https://forum.digikey.com/t/nanoedgeaistudio-an-automated-machine-learning-tool-for-stm32-developers/42631 "2024-06-27T07:10:31Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![abhijeet.sisodia](https://avatars.discourse-cdn.com/v4/letter/a/f04885/32.png) [@abhijeet.sisodia](https://forum.digikey.com/u/abhijeet.sisodia)\
**Post date:** [June 27, 2024, 7:10am UTC](https://forum.digikey.com/t/nanoedgeaistudio-an-automated-machine-learning-tool-for-stm32-developers/42631/1 "2024-06-27T07:10:31Z")

</div>

NanoEdgeAIStudio is a new Machine Learning (ML) technology which is a privilege to the developers by which they can create an optimal ML library based on a minimal amount of data. It is a PC based push-button development studio which can run on Windows, Linux Ubuntu.

 ![image](https://global.discourse-cdn.com/digikey/original/3X/8/d/8db365b7c4e224187165799b57a8449844ac390f.png)

The Studio can generate four types of libraries: anomaly detection, outlier detection, classification, and regression libraries. These libraries can be combined and chained to create a complete edge AI solution: anomaly or outlier detection to detect a problem on the equipment, classification to identify the source of the problem, and regression to extrapolate information and provide real insight to the maintenance team.

Multiple sensors can be combined either in a single library or using multiple libraries concurrently. This topology can respond to various types of input signals such as vibration and pressure, sound, magnetic, time of flight, etc.

Both learning and inference are done directly inside the microcontroller by means of the NanoEdge™ AI on-device learning library, which streamlines the edge AI process and significantly reduces development effort, cost and therefore time to market.

### All features

- Desktop tool for the design and generation of STM32-optimized libraries with small datasets:
  - _Anomaly detection libraries:_ Learn normality directly on the STM32 microcontroller and detect defects in real time
  - _One-class classification libraries:_ Perform the acquisition during normal equipment operation and detect any abnormal pattern deviation
  - _N-class classification libraries:_ Classify signals in real time
  - _Extrapolation libraries:_ Predict discrete values based on data patterns never seen before

- Support for any type of sensor for a variety of physical quantities: multi-axis acceleration, current, magnetic field, voltage, temperature, acoustic pressure, and more
- Millions of possible algorithms are available to find the optimal library in terms of accuracy, confidence, inference time, and memory footprint
- Generation of very small footprint libraries running down to the smallest Arm® Cortex®‑M0 microcontrollers
- Integrated tools such as:
  - Sampling finder tool to select the right data rate and the right data length easily
  - Datalogger generator to get ready to log data in a few clicks
  - Data manipulation tool for datasets
  - ML libraries benchmark to find the best combination between preprocessing and machine learning models
  - Embedded emulator to test library performance live with an attached STM32 board or from test data files
  - Inference time estimation to help users make an informed choice for model selection
  - Validation tool to compare the libraries given by NanoEdge™

There are various STM32 based products available with DigiKey supporting the NanoEdgeAI technology:

**SensorTile Wireless Industrial Node Development Kit**  
The STWIN.box (STEVAL-STWINBX1) is a development kit and reference design that simplifies prototyping and testing of advanced industrial sensing applications in IoT contexts such as condition monitoring and predictive maintenance.

The parts of this category available with DigiKey are [STEVAL-STWINBX1](https://www.digikey.com/en/products/detail/stmicroelectronics/STEVAL-STWINBX1/17879068), [STEVAL-STWINKT1B](https://www.digikey.com/en/products/detail/stmicroelectronics/STEVAL-STWINKT1B/13546585?s=N4IgTCBcDaIMoBUCiA1AggGQLSIOoEkA5AaQQEYAhEAXQF8g) and [STEVAL-MKBOXPRO](https://www.digikey.com/en/products/detail/stmicroelectronics/STEVAL-MKBOXPRO/19721662).

**Industrial sensor evaluation kit for condition monitoring based on the 2.4 GHz STM32WB5MMG module**  
The [STEVAL-PROTEUS1](https://www.digikey.com/en/products/detail/stmicroelectronics/STEVAL-PROTEUS1/16639758?s=N4IgTCBcDaIMoBUCiA1AggGQLQAUBKA8sgKpwCMIAugL5A) is an evaluation tool designed for temperature and vibration monitoring. It is based on a 2.4 GHz multiprotocol wireless SoC to address machine or facility condition monitoring for industrial applications.

The main board includes the STM32WB5MMG ultra-low-power and small form factor wireless radio module. This module is FCC and IC certified (FCC ID: YCP-STM32WB5M001 and IC: 8976A-STM32WB5M01).

**Discovery kit for IoT node with STM32U5 series**  
The [B-U585I-IOT02A](https://www.digikey.com/en/products/detail/stmicroelectronics/B-U585I-IOT02A/15218435?s=N4IgTCBcDaIEIFoCqBWAHCgkgzB5AKgAxgCCIAugL5A) Discovery kit provides a complete demonstration and development platform for the STM32U585AI microcontroller, featuring an Arm® Cortex®-M33 core with Arm® TrustZone® and Armv8-M mainline security extension, 2 Mbytes of Flash memory and 786 Kbytes of SRAM, as well as smart peripheral resources.

**Discovery kit with STM32H747XI MCU**  
The [STM32H747I-DISCO](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32H747I-DISCO/10244393?s=N4IgTCBcDaIMoBUCyBmMAJA7AFkwSQFoARPOAYQHkQBdAXyA) Discovery kit is a complete demonstration and development platform for STMicroelectronics STM32H747XIH6 microcontroller, designed to simplify user application development.

Some other NanoEdgeAIStudio supported STM32 development boards are:  
[STEVAL-STLKT01V1](https://www.digikey.com/en/products/detail/stmicroelectronics/STEVAL-STLKT01V1/6201099?s=N4IgTCBcDaIMoBUAyBpBAGAjANUyAugL5A), [STM32L562E-DK](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32L562E-DK/11501278?s=N4IgTCBcDaIMoBUCyBmMAZArANjAURAF0BfIA), [B-L475E-IOT01A1](https://www.digikey.com/en/products/detail/stmicroelectronics/B-L475E-IOT01A1/6615998), [STM32MP157FAC1](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157FAC1/11591173), [STM32MP157FAD1](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157FAD1/11591238), [STM32MP157FAA1](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157FAA1/11591134), [STM32MP157FAB1](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157FAB1/11591139), [STM32MP157F-DK2](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157F-DK2/13536968?s=N4IgTCBcDaIMoBUCyBmMSAKBGArAdgDEBaAEQGkIBdAXyA), [STM32MP157C-DK2](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157C-DK2/9990057?s=N4IgTCBcDaIMoBUCyBmMSAKBGArAdgGEBaAEQGkIBdAXyA), [STM32MP157AAC3T](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157AAC3T/10058594), [STM32MP157AAC3](https://www.digikey.com/en/products/detail/stmicroelectronics/STM32MP157AAC3/10238135).

> **Applicable Part Numbers**
>
> | DK Part # | | Mfr Part # |
> | --- | --- | --- |
> | 497-18230-ND | | STM32L412KBU6 |
> | 497-17957-ND | | STM32L431CBT6 |
> | 497-18229-ND | | STM32L412KBT6 |
> | 497-16579-ND | | STM32L433CCT6 |
> | 497-16586-ND | | STM32L443CCT6 |
> | 497-19376-2-ND,497-19376-1-ND,497-19376-6-ND | | STM32L431CBY7TR |
> | 497-16577-ND | | STM32L432KBU6 |
> | 497-17951-2-ND,497-17951-1-ND,497-17951-6-ND | | STM32L452REY6TR |
> | 497-17541-ND | | STM32L476RCT6 |
> | 497-17958-ND | | STM32L431KCU6 |
> | 497-19377-2-ND,497-19377-1-ND,497-19377-6-ND | | STM32L431CCU6TR |
> | 497-18830-2-ND,497-18830-1-ND,497-18830-6-ND | | STM32L431CCT6TR |
> | 497-17827-ND | | STM32L431CCT6 |
> | 497-16578-ND | | STM32L432KCU6 |
> | 497-17960-ND | | STM32L431RCT6 |
> | 497-16585-ND | | STM32L442KCU6 |
> | 497-19381-2-ND,497-19381-1-ND,497-19381-6-ND | | STM32L476RET6TR |
> | 497-STM32L433CCT3-ND | | STM32L433CCT3 |
> | 497-17982-ND | | STM32L452CCU6 |
> | 497-16582-ND | | STM32L433RCT6 |
> | 497-18596-ND | | STM32L432KCU3 |
> | 497-16584-ND | | STM32L433VCT6 |
> | 497-19378-2-ND,497-19378-1-ND,497-19378-6-ND | | STM32L433VCT6TR |
> | 497-17987-ND | | STM32L452VCI6 |
> | 497-17218-ND | | STM32L452CEU6 |
> | 497-15878-ND | | STM32L476VET6 |
> | 497-18835-2-ND,497-18835-1-ND,497-18835-6-ND | | STM32L451RET6TR |
> | 497-17735-2-ND,497-17735-1-ND,497-17735-6-ND | | STM32L486JGY6TR |
> | 497-STM32L452REI6-ND | | STM32L452REI6 |
> | 497-17219-ND | | STM32L452RET6 |
> | 497-19679-2-ND,497-19679-1-ND,497-19679-6-ND | | STM32L452RET6TR |
> | 497-17214-ND | | STM32L462RET6 |
> | 497-17102-ND | | STM32L496VGT6 |
> | 497-17981-ND | | STM32L451VET6 |
> | 497-17956-2-ND,497-17956-1-ND,497-17956-6-ND | | STM32L4A6VGY6PTR |
> | 497-STM32L4P5CGT6P-ND | | STM32L4P5CGT6P |
> | 497-17993-ND | | STM32L476QGI3 |
> | 497-17667-2-ND,497-17667-1-ND,497-17667-6-ND | | STM32L476JEY6TR |
> | 497-18964-ND | | STM32L476QEI6 |
> | 497-16387-ND | | STM32L471RGT6 |
> | 497-17539-2-ND,497-17539-1-ND,497-17539-6-ND | | STM32L476JGY6TR |
> | 497-16390-ND | | STM32L475RGT6 |
> | 497-17174-ND | | STM32L496VET6 |
> | 497-17540-ND | | STM32L476QGI6 |
> | 497-STM32L4Q5CGU6-ND | | STM32L4Q5CGU6 |
> | 497-17731-ND | | STM32L4A6RGT6 |
> | 497-STM32L4P5CGT6-ND | | STM32L4P5CGT6 |
> | 497-15877-ND | | STM32L476RGT6 |
> | 497-19382-2-ND,497-19382-1-ND,497-19382-6-ND | | STM32L476RGT6TR |
> | 497-16388-ND | | STM32L471VGT6 |
> | 497-15874-ND | | STM32L486RGT6 |
> | 497-STM32L4Q5RGT6-ND | | STM32L4Q5RGT6 |
> | 497-16391-ND | | STM32L475VGT6 |
> | 497-STM32L496VGY6TR-ND,497-STM32L496VGY6TRCT-ND,497-STM32L496VGY6TRDKR-ND | | STM32L496VGY6TR |
> | 497-STM32L476ZGT6TR-ND,497-STM32L476ZGT6CT-ND,497-STM32L476ZGT6DKR-ND | | STM32L476ZGT6TR |
> | 497-17542-ND | | STM32L476ZGT6 |
> | 497-17104-ND | | STM32L496QGI6 |
> | 497-17675-ND | | STM32L4R9AII6 |
> | 497-18339-2-ND,497-18339-1-ND,497-18339-6-ND | | STM32L496RGT6TR |
> | 497-17101-ND | | STM32L496RGT6 |
> | 497-17176-ND | | STM32L496ZET6 |
> | 497-STM32L4P5CGU6-ND | | STM32L4P5CGU6 |
> | 497-17173-ND | | STM32L496RGT3 |
> | 497-17733-ND | | STM32L4A6ZGT6 |
> | 497-17175-ND | | STM32L496VGT3 |
> | 497-17673-2-ND,497-17673-1-ND,497-17673-6-ND | | STM32L4R5ZIY6TR |
> | 497-18605-ND | | STM32L4R5VIT6 |
> | 497-18606-ND | | STM32L4S5VIT6 |
> | 497-17671-ND | | STM32L4R5QII6 |
> | 497-17674-ND | | STM32L4R7VIT6 |
> | 497-17672-ND | | STM32L4R5ZIT6 |
> | 497-19206-ND | | STM32L4R9ZGJ6 |
> | 497-19208-ND | | STM32L4S5ZIT6 |
> | 497-19210-ND | | STM32L4S9ZIJ6 |
> | 497-STM32L412K8U6-ND | | STM32L412K8U6 |
> | 497-STM32L412K8T6-ND | | STM32L412K8T6 |
> | 497-STM32L412C8T6-ND | | STM32L412C8T6 |
> | 497-18235-ND | | STM32L422KBT6 |
> | 497-18227-ND | | STM32L412CBT6 |
> | 497-18232-ND | | STM32L412RBT6 |
> | STM32L412RBT6P-ND | | STM32L412RBT6P |
> | 497-18594-ND | | STM32L431KBU3 |
> | 497-16580-ND | | STM32L433CCU6 |
> | 497-STM32L422TBY6TR-ND,497-STM32L422TBY6TRCT-ND,497-STM32L422TBY6TRDKR-ND | | STM32L422TBY6TR |
> | 497-18228-ND | | STM32L412CBU6 |
> | 497-16587-ND | | STM32L443CCU6 |
> | 497-17984-ND | | STM32L452RCT6 |
> | 497-18831-2-ND,497-18831-1-ND,497-18831-6-ND | | STM32L431KBU6TR |
> | 497-18595-ND | | STM32L431KBU6 |
> | 497-17849-ND | | STM32L431CBU6 |
> | 497-17966-ND | | STM32L433RCI3 |
> | 497-18597-ND | | STM32L451CEU6 |
> | 497-17979-ND | | STM32L451VCT6 |
> | 497-17967-ND | | STM32L433RCT3 |
> | 497-18963-ND | | STM32L475RCT6 |
> | 497-16837-ND | | STM32L431RBT6 |
> | 497-17838-ND | | STM32L431CCU6 |
> | 497-17538-ND | | STM32L471RET6 |
> | 497-17222-ND | | STM32L452VEI6 |
> | 497-17965-ND | | STM32L433RBT6 |
> | 497-17947-2-ND,497-17947-1-ND,497-17947-6-ND | | STM32L433RCY6TR |
> | 497-17985-ND | | STM32L452REI3 |
> | 497-15872-ND | | STM32L476RET6 |
> | 497-17948-2-ND,497-17948-1-ND,497-17948-6-ND | | STM32L443CCY6TR |
> | 497-17983-ND | | STM32L452RCI6 |
> | 497-17850-ND | | STM32L431VCT6 |
> | 497-16589-ND | | STM32L443RCT6 |
> | 497-17975-ND | | STM32L451RCT6 |
> | 497-17172-ND | | STM32L496RET6 |
> | 497-STM32L4P5CET6-ND | | STM32L4P5CET6 |
> | 497-16591-ND | | STM32L443VCT6 |
> | 497-17213-ND | | STM32L462CEU6 |
> | 497-17977-ND | | STM32L451RET6 |
> | 497-17954-2-ND,497-17954-1-ND,497-17954-6-ND | | STM32L476MGY6TR |
> | 497-19380-2-ND,497-19380-1-ND,497-19380-6-ND | | STM32L476QGI6TR |
> | 497-17992-ND | | STM32L476RGT3 |
> | 497-17955-2-ND,497-17955-1-ND,497-17955-6-ND | | STM32L496VGY6PTR |
> | 497-18598-ND | | STM32L452CEU3 |
> | 497-17729-ND | | STM32L4A6QGI6 |
> | 497-STM32L462VEI6-ND | | STM32L462VEI6 |
> | 497-17106-ND | | STM32L496AGI6 |
> | 497-STM32L475RCT3-ND | | STM32L475RCT3 |
> | 497-17730-ND | | STM32L4A6AGI6 |
> | 497-18599-ND | | STM32L452RET3 |
> | 497-STM32L471RGT6TR-ND,497-STM32L471RGT6CT-ND,497-STM32L471RGT6DKR-ND | | STM32L471RGT6TR |
> | 497-17835-ND | | STM32L476ZET6 |
> | 497-17543-ND | | STM32L486QGI6 |
> | 497-16842-ND | | STM32L476VGT7 |
> | 497-STM32L4P5VET6-ND | | STM32L4P5VET6 |
> | 497-15873-ND | | STM32L476VGT6 |
> | 497-STM32L4P5VGT6-ND | | STM32L4P5VGT6 |
> | 497-15875-ND | | STM32L486VGT6 |
> | 497-18053-ND | | STM32L4S9AII6 |
> | 497-17178-ND | | STM32L496ZGT6 |
> | 497-18604-ND | | STM32L4R5VGT6 |
> | 497-17678-ND | | STM32L4R9ZIT6 |
> | 497-STM32L496QGI3-ND | | STM32L496QGI3 |
> | 497-19204-ND | | STM32L4R5ZGT6 |
> | 497-19209-ND | | STM32L4S7VIT6 |
> | 497-19682-ND | | STM32L4R5ZIT6P |
> | 497-STM32L4R9ZIY6PTR-ND,497-STM32L4R9ZIY6PCT-ND,497-STM32L4R9ZIY6PDKR-ND | | STM32L4R9ZIY6PTR |
> | 497-17676-ND | | STM32L4R9VIT6 |
> | 497-STM32L4S7ZIT6-ND | | STM32L4S7ZIT6 |
> | 497-17677-ND | | STM32L4R9ZIJ6 |
> | STM32L412R8T6-ND | | STM32L412R8T6 |
> | 497-18234-ND | | STM32L422CBU6 |
> | 497-18233-ND | | STM32L422CBT6 |
> | 497-17942-2-ND,497-17942-1-ND,497-17942-6-ND | | STM32L431CCY6TR |
> | 497-17961-ND | | STM32L433CBT6 |
> | 497-18238-ND | | STM32L422RBT6 |
> | 497-17973-ND | | STM32L451CCU6 |
> | 497-17963-ND | | STM32L433CCU3 |
> | STM32L412CBT6P-ND | | STM32L412CBT6P |
> | 497-16581-ND | | STM32L433RCI6 |
> | 497-17976-ND | | STM32L451REI6 |
> | 497-18832-2-ND,497-18832-1-ND,497-18832-6-ND | | STM32L431RBT6TR |
> | 497-17840-ND | | STM32L476VCT6 |
> | 497-16838-ND | | STM32L431RCI6 |
> | 497-18601-ND | | STM32L475RET6 |
> | 497-19678-2-ND,497-19678-1-ND,497-19678-6-ND | | STM32L451CCU6TR |
> | 497-18600-ND | | STM32L471VET6 |
> | 497-17972-ND | | STM32L451CCU3 |
> | 497-17991-ND | | STM32L475VET6 |
> | 497-18834-2-ND,497-18834-1-ND,497-18834-6-ND | | STM32L433RCT6TR |
> | 497-17968-ND | | STM32L433RCT6P |
> | 497-16576-ND | | STM32L431VCI6 |
> | 497-STM32L4Q5CGT6-ND | | STM32L4Q5CGT6 |
> | 497-17980-ND | | STM32L451VEI6 |
> | 497-15876-ND | | STM32L486ZGT6 |
> | 497-19379-2-ND,497-19379-1-ND,497-19379-6-ND | | STM32L471VET6TR |
> | 497-16843-ND | | STM32L476ZGT3 |
> | 497-STM32L476ZET6TR-ND,497-STM32L476ZET6CT-ND,497-STM32L476ZET6DKR-ND | | STM32L476ZET6TR |
> | 497-17732-ND | | STM32L4A6VGT6 |
> | 497-19205-ND | | STM32L4R7ZIT6 |
> | 497-19383-2-ND,497-19383-1-ND,497-19383-6-ND | | STM32L476VGT6TR |
> | 497-17994-ND | | STM32L476VGT3 |
> | 497-19384-2-ND,497-19384-1-ND,497-19384-6-ND | | STM32L486VGT6TR |
> | 497-17999-ND | | STM32L496ZGT6P |
> | 497-17998-ND | | STM32L496QGI6P |
> | 497-17959-ND | | STM32L431RBI6 |
> | 497-17943-2-ND,497-17943-1-ND,497-17943-6-ND | | STM32L431RBY6TR |
> | 497-17969-ND | | STM32L433VCI3 |
> | 497-17970-ND | | STM32L433VCT3 |
> | 497-17216-ND | | STM32L462VET6 |
> | 497-STM32L443RCT6TR-ND,497-STM32L443RCT6TRCT-ND,497-STM32L443RCT6TRDKR-ND | | STM32L443RCT6TR |
> | 497-17950-2-ND,497-17950-1-ND,497-17950-6-ND | | STM32L451REY6TR |
> | 497-STM32L4Q5CGT6P-ND | | STM32L4Q5CGT6P |
> | 497-17990-ND | | STM32L471VGT3 |
> | 497-18602-ND | | STM32L486RGT7 |
> | 497-STM32L4A6VGT6P-ND | | STM32L4A6VGT6P |
> | 497-STM32L475RET6TR-ND,497-STM32L475RET6TRCT-ND,497-STM32L475RET6TRDKR-ND | | STM32L475RET6TR |
> | 497-STM32L4Q5VGT6P-ND | | STM32L4Q5VGT6P |
> | 497-STM32L4Q5VGT6-ND | | STM32L4Q5VGT6 |
> | 497-STM32L462VET6TR-ND,497-STM32L462VET6TRCT-ND,497-STM32L462VET6TRDKR-ND | | STM32L462VET6TR |
> | 497-17996-ND | | STM32L486ZGT3 |
> | 497-STM32L496AGI3-ND | | STM32L496AGI3 |
> | 497-STM32L486RGT7TR-ND,497-STM32L486RGT7TRCT-ND,497-STM32L486RGT7TRDKR-ND | | STM32L486RGT7TR |
> | 497-STM32L412C8U6-ND | | STM32L412C8U6 |
> | 497-STM32L412CBU6TR-ND,497-STM32L412CBU6TRCT-ND,497-STM32L412CBU6TRDKR-ND | | STM32L412CBU6TR |
> | 497-STM32L412CBT6TR-ND,497-STM32L412CBT6TRCT-ND,497-STM32L412CBT6TRDKR-ND | | STM32L412CBT6TR |
> | 497-STM32L412KBU3-ND | | STM32L412KBU3 |
> | 497-STM32L412KBU3TR-ND,497-STM32L412KBU3TRCT-ND,497-STM32L412KBU3TRDKR-ND | | STM32L412KBU3TR |
> | 497-17952-2-ND,497-17952-1-ND,497-17952-6-ND | | STM32L462REY6TR |
> | 497-18237-ND | | STM32L422RBI6 |
> | 497-STM32L433CBT7TR-ND,497-STM32L433CBT7CT-ND,497-STM32L433CBT7DKR-ND | | STM32L433CBT7 |
> | 497-STM32L433CCT6TR-ND,497-STM32L433CCT6TRCT-ND,497-STM32L433CCT6TRDKR-ND | | STM32L433CCT6TR |
> | 497-STM32L4P5RET6-ND | | STM32L4P5RET6 |
> | 497-17215-ND | | STM32L462REI6 |
> | 497-STM32L471ZGJ6-ND | | STM32L471ZGJ6 |
> | 497-17989-ND | | STM32L471QEI6 |
> | 497-17170-ND | | STM32L496QEI6 |
> | 497-17997-ND | | STM32L496AGI6P |
> | 497-STM32L4Q5ZGT6P-ND | | STM32L4Q5ZGT6P |
> | 497-STM32L476MGY6MTR-ND,497-STM32L476MGY6MTRCT-ND,-1138-STM32L476MGY6MTRDKR-ND,497-STM32L476MGY6MTRDKR-ND | | STM32L476MGY6MTR |
> | 497-18231-ND | | STM32L412RBI6 |
> | 497-STM32L4A6RGT7TR-ND,497-STM32L4A6RGT7TRCT-ND,-1138-STM32L4A6RGT7TRDKR-ND,497-STM32L4A6RGT7TRDKR-ND | | STM32L4A6RGT7TR |
> | 497-STM32L443RCI6-ND | | STM32L443RCI6 |
> | 497-STM32L452CET6-ND | | STM32L452CET6 |
> | 497-19203-ND | | STM32L4R5QGI6 |
> | 497-STM32L496VGT6P-ND | | STM32L496VGT6P |
> | 497-16386-ND | | STM32L471QGI6 |
> | 497-STM32L486QGI6TR-ND,497-STM32L486QGI6TRCT-ND,497-STM32L486QGI6TRDKR-ND | | STM32L486QGI6TR |
> | 497-18055-ND | | STM32L4S5QII6 |
> | 497-STM32L4S9ZIY6TR-ND,497-STM32L4S9ZIY6TRCT-ND,497-STM32L4S9ZIY6TRDKR-ND | | STM32L4S9ZIY6TR |
> | 497-STM32L431RCT6TR-ND,497-STM32L431RCT6CT-ND,497-STM32L431RCT6DKR-ND | | STM32L431RCT6TR |
> | 497-17177-ND | | STM32L496ZGT3 |
> | 497-17221-ND | | STM32L452VET6 |
> | 497-STM32L4P5ZGT6-ND | | STM32L4P5ZGT6 |
> | 497-17988-ND | | STM32L452VCT6 |
> | 497-17986-ND | | STM32L452RET6P |
> | 497-19680-ND | | STM32L475VCT6 |
> | 497-16389-ND | | STM32L471ZGT6 |
> | 497-STM32L4S9ZIT6-ND | | STM32L4S9ZIT6 |
> | 497-17962-ND | | STM32L433CBU6 |
> | 497-18236-ND | | STM32L422KBU6 |
> | 497-17974-ND | | STM32L451RCI6 |
> | 497-17978-ND | | STM32L451VCI6 |
> | 497-16590-ND | | STM32L443VCI6 |
> | 497-16839-ND | | STM32L443RCI3 |
> | 497-17946-2-ND,497-17946-1-ND,497-17946-6-ND | | STM32L433RBY6TR |
> | 497-17944-2-ND,497-17944-1-ND,497-17944-6-ND | | STM32L431RCY6TR |
> | 497-17945-2-ND,497-17945-1-ND,497-17945-6-ND | | STM32L433CCY6TR |
> | 497-STM32L4P5CEU6-ND | | STM32L4P5CEU6 |
> | 497-17922-ND | | STM32L471ZET6 |
> | 497-18603-ND | | STM32L4A6RGT7 |
> | 497-18000-ND | | STM32L4A6AGI6P |
> | 497-STM32L4Q5CGU6P-ND | | STM32L4Q5CGU6P |
> | 497-17168-ND | | STM32L496AEI6 |
> | 497-17953-2-ND,497-17953-1-ND,497-17953-6-ND | | STM32L476MEY6TR |
> | 497-STM32L4P5VGT6P-ND | | STM32L4P5VGT6P |
> | 497-STM32L4P5AGI6-ND | | STM32L4P5AGI6 |
> | 497-STM32L4P5AGI6P-ND | | STM32L4P5AGI6P |
> | 497-STM32L4Q5AGI6-ND | | STM32L4Q5AGI6 |
> | STM32L4R9VGT6-ND | | STM32L4R9VGT6 |
> | 497-18056-ND | | STM32L4R5AGI6 |
> | 497-18054-ND | | STM32L4R9AGI6 |
> | 497-STM32L4P5ZGT6P-ND | | STM32L4P5ZGT6P |
> | 497-19207-ND | | STM32L4R9ZGT6 |
> | 497-STM32L412K8U6TR-ND | | STM32L412K8U6TR |
> | 497-STM32L412C8U6TR-ND | | STM32L412C8U6TR |
> | 497-STM32L412K8T6TR-ND | | STM32L412K8T6TR |
> | STM32L412TBY6PTR-ND | | STM32L412TBY6PTR |
> | STM32L412TBY6TR-ND | | STM32L412TBY6TR |
> | 497-STM32L412KBU6TR-ND | | STM32L412KBU6TR |
> | 497-STM32L412TBY3TR-ND | | STM32L412TBY3TR |
> | STM32L431CBY6TR-ND | | STM32L431CBY6TR |
> | STM32L412CBU6P-ND | | STM32L412CBU6P |
> | STM32L412R8I6-ND | | STM32L412R8I6 |
> | 497-STM32L412R8T6TR-ND | | STM32L412R8T6TR |
> | STM32L431CBU6TR-ND | | STM32L431CBU6TR |
> | 497-STM32L431CBT6TR-ND | | STM32L431CBT6TR |
> | 497-STM32L412KBT3TR-ND | | STM32L412KBT3TR |
> | STM32L431RBI6TR-ND | | STM32L431RBI6TR |
> | STM32L433CBY6TR-ND | | STM32L433CBY6TR |
> | STM32L412RBI6P-ND | | STM32L412RBI6P |
> | 497-STM32L412CBT3TR-ND | | STM32L412CBT3TR |
> | STM32L432KBU6TR-ND | | STM32L432KBU6TR |
> | 497-STM32L412KBT3-ND | | STM32L412KBT3 |
> | 497-STM32L412RBT6TR-ND | | STM32L412RBT6TR |
> | 497-STM32L431KBU3TR-ND | | STM32L431KBU3TR |
> | STM32L431KCU6TR-ND | | STM32L431KCU6TR |
> | 497-STM32L412CBT3-ND | | STM32L412CBT3 |
> | STM32L422RBT6P-ND | | STM32L422RBT6P |
> | 497-STM32L431CBT3TR-ND | | STM32L431CBT3TR |
> | 497-STM32L451CEU6TR-ND,497-STM32L451CEU6TRCT-ND,-1138-STM32L451CEU6TRDKR-ND,497-STM32L451CEU6TRDKR-ND | | STM32L451CEU6TR |
> | 497-STM32L431RCI6TR-ND | | STM32L431RCI6TR |
> | 497-17964-ND | | STM32L433RBI6 |
> | 497-STM32L431CCU7TR-ND | | STM32L431CCU7TR |
> | 497-STM32L431CBT3-ND | | STM32L431CBT3 |
> | 497-STM32L412RBT3-ND | | STM32L412RBT3 |
> | STM32L431RBI3-ND | | STM32L431RBI3 |
> | 497-STM32L443CCF6TR-ND | | STM32L443CCF6TR |
> | 497-STM32L433CCU6TR-ND | | STM32L433CCU6TR |
> | 497-STM32L431CCU7-ND | | STM32L431CCU7 |
> | STM32L442KCU6TR-ND | | STM32L442KCU6TR |
> | STM32L433RCI6TR-ND | | STM32L433RCI6TR |
> | 497-STM32L451RCI6TR-ND | | STM32L451RCI6TR |
> | 497-STM32L443CCT6TR-ND | | STM32L443CCT6TR |
> | STM32L443RCI6TR-ND | | STM32L443RCI6TR |
> | STM32L433CCY3TR-ND | | STM32L433CCY3TR |
> | STM32L433RCY3TR-ND | | STM32L433RCY3TR |
> | 497-STM32L432KCU3TR-ND | | STM32L432KCU3TR |
> | 497-STM32L433CCU3TR-ND | | STM32L433CCU3TR |
> | STM32L451CCU3TR-ND | | STM32L451CCU3TR |
> | 497-STM32L433CCT3TR-ND | | STM32L433CCT3TR |
> | 497-STM32L431VCT6TR-ND | | STM32L431VCT6TR |
> | 497-STM32L431VCI7-ND | | STM32L431VCI7 |
> | 497-STM32L431VCI7TR-ND | | STM32L431VCI7TR |
> | 497-STM32L452RCT6TR-ND | | STM32L452RCT6TR |
> | 497-16583-ND | | STM32L433VCI6 |
> | 497-STM32L433VCI6TR-ND | | STM32L433VCI6TR |
> | 497-STM32L443RCI3TR-ND | | STM32L443RCI3TR |
> | 497-STM32L451REI6TR-ND | | STM32L451REI6TR |
> | 497-STM32L431VCI3-ND | | STM32L431VCI3 |
> | 497-STM32L431VCI3TR-ND | | STM32L431VCI3TR |
> | STM32L452REY6PTR-ND | | STM32L452REY6PTR |
> | 497-STM32L433RCT3TR-ND | | STM32L433RCT3TR |
> | 497-STM32L451CET6-ND | | STM32L451CET6 |
> | 497-STM32L451RCT3-ND | | STM32L451RCT3 |
> | 497-STM32L451RCT3TR-ND | | STM32L451RCT3TR |
> | 497-STM32L443VCT6TR-ND | | STM32L443VCT6TR |
> | STM32L462CEU6TR-ND | | STM32L462CEU6TR |
> | 497-STM32L462CEU6F-ND | | STM32L462CEU6F |
> | STM32L476RCT6TR-ND | | STM32L476RCT6TR |
> | 497-STM32L462CET6-ND | | STM32L462CET6 |
> | STM32L475RCT7-ND | | STM32L475RCT7 |
> | STM32L475RCT7TR-ND | | STM32L475RCT7TR |
> | 497-STM32L462RET6TR-ND | | STM32L462RET6TR |
> | 497-STM32L471RET6TR-ND | | STM32L471RET6TR |
> | 497-STM32L452VEI6TR-ND | | STM32L452VEI6TR |
> | 497-STM32L451VET6TR-ND | | STM32L451VET6TR |
> | STM32L462VEI6TR-ND | | STM32L462VEI6TR |
> | STM32L476VCT6TR-ND | | STM32L476VCT6TR |
> | STM32L471QEI6TR-ND | | STM32L471QEI6TR |
> | 497-STM32L471RET3-ND | | STM32L471RET3 |
> | 497-STM32L471RET3TR-ND | | STM32L471RET3TR |
> | 497-STM32L4P5VEY6TR-ND | | STM32L4P5VEY6TR |
> | STM32L452VEI3-ND | | STM32L452VEI3 |
> | 497-STM32L452VEI3TR-ND | | STM32L452VEI3TR |
> | 497-STM32L475VET6TR-ND | | STM32L475VET6TR |
> | STM32L476VET6TR-ND | | STM32L476VET6TR |
> | STM32L471QEI7-ND | | STM32L471QEI7 |
> | STM32L471QEI7TR-ND | | STM32L471QEI7TR |
> | STM32L476JGY6PTR-ND | | STM32L476JGY6PTR |
> | STM32L476QEI6TR-ND | | STM32L476QEI6TR |
> | 497-STM32L496RET6TR-ND | | STM32L496RET6TR |
> | STM32L476JGY7TR-ND | | STM32L476JGY7TR |
> | 497-STM32L471QEI3-ND | | STM32L471QEI3 |
> | 497-STM32L471QEI3TR-ND | | STM32L471QEI3TR |
> | 497-STM32L496ZGT6TR-ND,497-STM32L496ZGT6TRCT-ND,-1138-STM32L496ZGT6TRDKR-ND,497-STM32L496ZGT6TRDKR-ND | | STM32L496ZGT6TR |
> | 497-STM32L496WGY6PTR-ND | | STM32L496WGY6PTR |
> | 497-STM32L475RGT6TR-ND | | STM32L475RGT6TR |
> | 497-STM32L496VET6TR-ND | | STM32L496VET6TR |
> | 497-STM32L496QEI6TR-ND | | STM32L496QEI6TR |
> | STM32L4A6VGY6TR-ND | | STM32L4A6VGY6TR |
> | STM32L471VGT6TR-ND | | STM32L471VGT6TR |
> | 497-STM32L471QGI6TR-ND | | STM32L471QGI6TR |
> | 497-STM32L476JGY3TR-ND | | STM32L476JGY3TR |
> | STM32L452VET3-ND | | STM32L452VET3 |
> | 497-STM32L4P5VGY6TR-ND | | STM32L4P5VGY6TR |
> | 497-STM32L4P5VGY6PTR-ND | | STM32L4P5VGY6PTR |
> | STM32L486RGT6TR-ND | | STM32L486RGT6TR |
> | 497-17949-2-ND,497-17949-1-ND,497-17949-6-ND | | STM32L443RCY6TR |
> | 497-STM32L476MGY3TR-ND | | STM32L476MGY3TR |
> | 497-STM32L4P5VET6TR-ND | | STM32L4P5VET6TR |
> | 497-STM32L4Q5VGY6TR-ND | | STM32L4Q5VGY6TR |
> | 497-STM32L4Q5VGY6PTR-ND | | STM32L4Q5VGY6PTR |
> | 497-STM32L4P5QEI6-ND | | STM32L4P5QEI6 |
> | STM32L475RGT7-ND | | STM32L475RGT7 |
> | STM32L475RGT7TR-ND | | STM32L475RGT7TR |
> | STM32L471ZEJ6-ND | | STM32L471ZEJ6 |
> | STM32L471ZEJ6TR-ND | | STM32L471ZEJ6TR |
> | STM32L471ZET6TR-ND | | STM32L471ZET6TR |
> | STM32L476QGI6P-ND | | STM32L476QGI6P |
> | 497-STM32L4P5AEI6-ND | | STM32L4P5AEI6 |
> | STM32L496RGT6P-ND | | STM32L496RGT6P |
> | 497-STM32L4P5CGU6P-ND | | STM32L4P5CGU6P |
> | STM32L4A6RGT6P-ND | | STM32L4A6RGT6P |
> | STM32L4A6RGT6TR-ND | | STM32L4A6RGT6TR |
> | 497-STM32L476VGT7TR-ND | | STM32L476VGT7TR |
> | 497-STM32L4P5RGT6-ND | | STM32L4P5RGT6 |
> | 497-STM32L4P5RGT6P-ND | | STM32L4P5RGT6P |
> | STM32L496VGT6TR-ND | | STM32L496VGT6TR |
> | 497-STM32L496QGI6S-ND | | STM32L496QGI6S |
> | 497-STM32L496QGI6STR-ND | | STM32L496QGI6STR |
> | 497-STM32L4Q5RGT6P-ND | | STM32L4Q5RGT6P |
> | 497-STM32L4A6VGT6PTR-ND | | STM32L4A6VGT6PTR |
> | 497-STM32L4A6VGT6TR-ND | | STM32L4A6VGT6TR |
> | 497-18001-ND | | STM32L4A6QGI6P |
> | 497-STM32L471ZEJ3-ND | | STM32L471ZEJ3 |
> | 497-STM32L471ZEJ3TR-ND | | STM32L471ZEJ3TR |
> | 497-STM32L496VET3-ND | | STM32L496VET3 |
> | STM32L4R5ZGY6TR-ND | | STM32L4R5ZGY6TR |
> | 497-STM32L4P5VGT6TR-ND | | STM32L4P5VGT6TR |
> | 497-STM32L4P5QGI6P-ND | | STM32L4P5QGI6P |
> | 497-STM32L4P5QGI6-ND | | STM32L4P5QGI6 |
> | 497-STM32L4P5QGI6STR-ND | | STM32L4P5QGI6STR |
> | 497-STM32L4P5QGI6TR-ND | | STM32L4P5QGI6TR |
> | 497-STM32L4P5QGI6S-ND | | STM32L4P5QGI6S |
> | 497-STM32L476QGI3TR-ND | | STM32L476QGI3TR |
> | 497-STM32L4A6AGI6TR-ND | | STM32L4A6AGI6TR |
> | 497-STM32L4Q5QGI6-ND | | STM32L4Q5QGI6 |
> | 497-STM32L4Q5QGI6P-ND | | STM32L4Q5QGI6P |
> | 497-STM32L4Q5RGT3-ND | | STM32L4Q5RGT3 |
> | 497-STM32L486VGT3TR-ND | | STM32L486VGT3TR |
> | 497-STM32L496RGT3TR-ND | | STM32L496RGT3TR |
> | 497-STM32L496ZET6TR-ND | | STM32L496ZET6TR |
> | 497-STM32L4Q5AGI6P-ND | | STM32L4Q5AGI6P |
> | STM32L4R5QGI6TR-ND | | STM32L4R5QGI6TR |
> | 497-STM32L4R5QGI6STR-ND | | STM32L4R5QGI6STR |
> | 497-STM32L4R5QGI6S-ND | | STM32L4R5QGI6S |
> | STM32L476ZGJ6-ND | | STM32L476ZGJ6 |
> | 497-STM32L4P5ZET6-ND | | STM32L4P5ZET6 |
> | STM32L4R9ZGY6TR-ND | | STM32L4R9ZGY6TR |
> | STM32L486VGT3-ND | | STM32L486VGT3 |
> | STM32L4S5ZIY6TR-ND | | STM32L4S5ZIY6TR |
> | 497-STM32L4P5ZGT6TR-ND | | STM32L4P5ZGT6TR |
> | STM32L4R5QII6P-ND | | STM32L4R5QII6P |
> | 497-STM32L4R5QII6TR-ND | | STM32L4R5QII6TR |
> | 497-STM32L4R5VIT6TR-ND | | STM32L4R5VIT6TR |
> | STM32L4R7AII6-ND | | STM32L4R7AII6 |
> | 497-STM32L4S5VIT6TR-ND | | STM32L4S5VIT6TR |
> | 497-18002-ND | | STM32L4A6ZGT6P |
> | STM32L4R5AII6-ND | | STM32L4R5AII6 |
> | STM32L4R5AII6P-ND | | STM32L4R5AII6P |
> | 497-STM32L4R5ZGT6TR-ND | | STM32L4R5ZGT6TR |
> | STM32L4S5AII6-ND | | STM32L4S5AII6 |
> | 497-STM32L4Q5ZGT6-ND | | STM32L4Q5ZGT6 |
> | STM32L4S5QII3P-ND | | STM32L4S5QII3P |
> | STM32L4S7AII6-ND | | STM32L4S7AII6 |
> | 497-STM32L4S5AII3-ND | | STM32L4S5AII3 |
> | 497-STM32L4S5AII3TR-ND | | STM32L4S5AII3TR |
> | 497-STM32L4S5VIT3-ND | | STM32L4S5VIT3 |
> | STM32L4S9VIT6-ND | | STM32L4S9VIT6 |
> | 497-STM32L4S9ZIJ6TR-ND | | STM32L4S9ZIJ6TR |
> | 497-17679-2-ND,497-17679-1-ND,497-17679-6-ND | | STM32L4R9ZIY6TR |
> | STM32L476JGY6VTR-ND | | STM32L476JGY6VTR |
> | STM32L451RCY6TR-ND | | STM32L451RCY6TR |
> | STM32L452RCY6TR-ND | | STM32L452RCY6TR |
> | STM32L476JGY6UTR-ND | | STM32L476JGY6UTR |
> | STM32L476VGT6U-ND | | STM32L476VGT6U |
> | STM32L476ZGT6U-ND | | STM32L476ZGT6U |
> | STM32L476JEY6VTR-ND | | STM32L476JEY6VTR |
> | 497-STM32U585AII6Q-ND | | STM32U585AII6Q |
> | 497-STM32U585AII6-ND | | STM32U585AII6 |
> | 497-STM32U585AII6TR-ND | | STM32U585AII6TR |
> | 497-STM32U585AII6QTR-ND | | STM32U585AII6QTR |
> | 497-STM32U585AII3-ND | | STM32U585AII3 |
> | 497-17675-ND | | STM32L4R9AII6 |
> | 497-19206-ND | | STM32L4R9ZGJ6 |
> | 497-17678-ND | | STM32L4R9ZIT6 |
> | 497-STM32L4R9ZIY6PTR-ND,497-STM32L4R9ZIY6PCT-ND,497-STM32L4R9ZIY6PDKR-ND | | STM32L4R9ZIY6PTR |
> | 497-17676-ND | | STM32L4R9VIT6 |
> | 497-17677-ND | | STM32L4R9ZIJ6 |
> | STM32L4R9VGT6-ND | | STM32L4R9VGT6 |
> | 497-18054-ND | | STM32L4R9AGI6 |
> | 497-19207-ND | | STM32L4R9ZGT6 |
> | STM32L4R9ZGY6TR-ND | | STM32L4R9ZGY6TR |
> | 497-17679-2-ND,497-17679-1-ND,497-17679-6-ND | | STM32L4R9ZIY6TR |
> | 497-STM32U585AII6Q-ND | | STM32U585AII6Q |
> | 497-STM32U585AII6-ND | | STM32U585AII6 |
> | 497-STM32U585AII6TR-ND | | STM32U585AII6TR |
> | 497-STM32U585AII6QTR-ND | | STM32U585AII6QTR |
> | 497-STM32U585AII3-ND | | STM32U585AII3 |
> | 497-17878-2-ND, 497-17878-1-ND, 497-17878-6-ND | | LD39115J18R |