Need 13 meters of the product FP014C-R5-ND. Could you please confirm if this product c

------Question for FP-301 1/4" CR 200’ Please Put your question below------


I need 13 meters of the product FP014C-R5-ND.Could you please confirm if this product comes in rolls? If so, could you let me know how many rolls I would need to order to cover 13 meters? Could you provide the price per meter?

Hello s.craddock,

Welcome to the DigiKey TechForum.

These have a minimum order quantity of 50, and each piece is 0.50" long which is 12.7mm. We do not provide these in rolls no.

Hello s.craddock,
We do have part 19-FP301-1/4-100’-CLEAR-SPOOL-ND it is the same series under a different part number it is 100 feet or 30.5 meters long it is in stock and you can request a quote from quotes@digikey.com for 1 full spool.

Hi s.craddock,

You can also order the following part number:

The “DS” suffix refers to “Digi-Spool”, which is how we call out a continuous spool which is cut to the length you require. You call out the number of feet you need and we cut to that length.

To convert from meters to feet, multiply by 3.281 and round up. So you would need 43ft (3.281 x meters = ft).

Looks like it would be more expensive on a per-unit basis than the 100ft (30.5m) length part @Quinn_2289 mentions, 19-FP301-1/4-100’-CLEAR-SPOOL-ND, but you wouldn’t be paying for the extra length you don’t need then.