We have a 8-pin flat connector for a Cyberpower PR1500LCD display panel. We need a part number for the pair or just the mail part
Hello cecyoung, Welcome to the DigiKey TechForum.
I was unable to find any specifications on this type of connector for the PR1500LCD display but we can still try to find you a connector that works but will need some more information. Can you measure the pitch of this connector, that will be the first thing we want to know. I provided a link showing you how to find the pitch of a connector below:
Pitch of a Connector
If you are also able to provide us with the wire gauge and the contact type of this connector, we should be able to get you a better answer.
Here is a diagram. This is a single inline 8-pin male connector.
I trust this diagram is satisfactory.
If you have any questions, please do not hesitate to contact me
Thank you and have a great day.
Mr. Cecil Young
Technology Professional
SBG Innovative Technologies Corp.
I found the S9432-ND
It looks close
This part costs $0.10 and $7.99 for shipping. Is this being shipped from the USA? Is there a Canadian supplier?
It would be shipped from Minnesota, USA.
Nathan, thanks for the guidance earlier. On the order90549622, we purchase 455-11989-ND and S9432-ND housings. Both fit the onboard connector on the part we are repairing. Now I need the contacts
For these Housings:
(1) Housing S9432-ND (Sullins SWH201-NULN-S08-UU-WH)
Contact SWT201-UPTN-S01-UU-UU (Sullins) (TIN) 98,364 in stock
I do not know what the 24 means in β24-28AWG Crimp TINβ
(2) Housing: 455-1189-ND (PHR-8)
Contact: SPH-002-P0.5S TIN (no stock)
My wire stripper goes down to 20AWG for stranded wire. The wire I am repairing is a bit smaller. I would guess it is between 24AWG - 26AWG. The wire is stranded.