New custom SiTime part request please

I’d like to order SiTime part number SiT3372AI-2EH-33NB145.96000.
Is it possible to add this to your website ? If this series is not possible then a VCXO in the SiT3342 would also work. Thank you
David

Hello g0mrf,

Welcome to the DigiKey TechForum! We are not able to add the SiT3372AI-2EH-33NB145.96000 to the website, however we may have an option to add SiT3372AE-2EH-33NB145.96000 instead. The E denotes a -40 to 105° which does cover the -40 to 85° of the I. Would you like to see if we can try to add this one?

Hi Klint_12443

Excellent. I thought the -40 to +85 would be easier for you, but your choice of part has a better specification.

So, yes please the SiT3372AE-2EH-33NB145.96000 will be perfect.

Thank you, it’s great to see custom SiTime products available after the Silicon Labs range was discontinued.

David

Hello g0mrf,

I wanted to give a quick heads up that we’re working on this one yet and I hope to update you when we reach the next steps.

Regards,
Klint

Thank you Klint.

Hopefully the unprogrammed blanks are in the building.

Much appreciated

David

Hello g0mrf,

Good news, the part is on our website. It should be available to purchase within 3 days, you’ll want to check back periodically.

1473-SiT3372AE-2EH-33NB145.96000-ND

Regards,
Klint Mahne