------Question for 55025-01 Please Put your question below------
Is this type of switch available with no toggle. Just ON - OFF in different position. I have a customer request that needs to see/visual the level, if the switch is on or off position.
------Question for 55025-01 Please Put your question below------
Is this type of switch available with no toggle. Just ON - OFF in different position. I have a customer request that needs to see/visual the level, if the switch is on or off position.
The customer would be wanting markings on the switch? Or they would like this switch but the switch would maintain it’s position when toggled?
For the option that maintains the F8824-ND was found.
55025 Cole Hersee | Switches | DigiKey
They can then also use the 432-1241-ND to have the ON OFF marking when mounting the switch.
272-06747 Carling Technologies | Switches | DigiKey
Hello Nathan.
The switch is a toggle type. That goes on (short circuit) momentary and then permanently OFF, we need this type of enclosure but the switch to go permanently ON and permanently OFF.
Then the switch I had provided above would work.
Thanks Nathan. I will check it out asap. Thanks for your support.
The switch has to be permanently OFF and permanetly ON. and to be visuabel on the swicth the position.
They call a switch that stays in the position it is actuated ‘latching’. If the switch indicates in DigiKey’s system that it is On-Off it would be a latching switch. The part number Nathan provided F8824-ND would latch into the position it is moved to, or permanent, as you call it.
Ok Kristof, thank you. Is now in my basket…![]()