Parasitic capacitance between two screw connector terminals?

------Question for 691137710002 Please Put your question below------

What is the parasitic capacitance between two screw connector terminals on the 691137710002?

I estimate it to be on the order of 5 pF looking at the dimensions and insulator material in the datasheet. C = (3.8ɛo)(7mm ⋅ 11mm) / 0.7mm. If that’s the right order of magnitude, then great! If the capacitance significantly higher than this, I’ll have to settle for removing solder and resoldering everytime I want to switch out the inductor for my unclamped inductive stress test.

Hello allbrand,

Welcome to the DigiKey TechForum.

I have sent a request for our engineers to take a look at this. We will get back to you as soon as we can. If anyone else knows the answer, they can post it here as well.

1 Like

Greetings,

5pF would seem like a reasonable guesstimate to me, though since it’s not characterized for the part it’s the sort of figure that one would do well to characterize/validate for oneself.

1 Like