Part id

Hi all ,new to this site and this electronics endeavor of mine ! Please be patient!!

I have a Clíp similar to I guess a push down connector!! This application is used specifically on a ford EATC module and more specific each of the 4 solenoids/actuators inside of the unit each has two wire mounting ports that a wire is pushed into and the (clips) Im trying to source are then are used to further push the wire in to the slot to prevent coming loose and it also appears the action causes Pearcing of the wire insulation to then make connect completing the connection

First pic is of the 4 solenoids inside the eatc

Second pic is of the Clíps Im referring to the dimensions are roughly 5mm wide and about 6mm in height

Last pic is of the individual solenoid and the two small wire termination points in which the Clíp is then inserted to affix the wire

Hello @pochebnicky

The clip you describe is an insulation displacement contact (IDC). I cannot confirm any of these will fit, so please send a clear, in-focus and multiple angled photos of the clip. A better shot of the solenoids might help too.

In the meantime, I suggest reviewing these parts linked HERE.

The clip photo vaguely represents something like 2-1601140-1.