PocketBeagle Getting Started


#1

This is a page about TI’s Cortex-A8 based; PocketBeagle.

Table of Contents:

Availability

Boards:

Click Boards:

Basic Requirements

ARM Cross Compiler: GCC

This is a pre-built (64bit) version of Linaro GCC that runs on generic linux, sorry (32bit) x86 users, it’s time to upgrade…
Download/Extract:

#~/
wget -c https://releases.linaro.org/components/toolchain/binaries/6.4-2018.05/arm-linux-gnueabihf/gcc-linaro-6.4.1-2018.05-x86_64_arm-linux-gnueabihf.tar.xz
tar xf gcc-linaro-6.4.1-2018.05-x86_64_arm-linux-gnueabihf.tar.xz
export CC=`pwd`/gcc-linaro-6.4.1-2018.05-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-

Test Cross Compiler:

#~/
${CC}gcc --version
arm-linux-gnueabihf-gcc (Linaro GCC 6.4-2018.05) 6.4.1 20180425 [linaro-6.4-2018.05 revision 7b15d0869c096fe39603ad63dc19ab7cf035eb70]
Copyright (C) 2017 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

Bootloader: U-Boot

Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
eewiki.net patch archive: https://github.com/eewiki/u-boot-patches
Download:

#~/
git clone https://github.com/u-boot/u-boot
cd u-boot/
git checkout v2018.09-rc2 -b tmp

Patches:

#~/u-boot
wget -c https://rcn-ee.com/repos/git/u-boot-patches/v2018.09-rc2/0001-am335x_evm-uEnv.txt-bootz-n-fixes.patch
wget -c https://rcn-ee.com/repos/git/u-boot-patches/v2018.09-rc2/0002-U-Boot-BeagleBone-Cape-Manager.patch
 
patch -p1 < 0001-am335x_evm-uEnv.txt-bootz-n-fixes.patch
patch -p1 < 0002-U-Boot-BeagleBone-Cape-Manager.patch

Configure and Build:

#~/u-boot
make ARCH=arm CROSS_COMPILE=${CC} distclean
make ARCH=arm CROSS_COMPILE=${CC} am335x_evm_defconfig
make ARCH=arm CROSS_COMPILE=${CC}

Linux Kernel

This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.

TI BSP

Download:

#~/
git clone https://github.com/RobertCNelson/ti-linux-kernel-dev.git
cd ti-linux-kernel-dev/

For TI v4.14.x:

#~/ti-linux-kernel-dev/
git checkout origin/ti-linux-4.14.y -b tmp

For TI v4.14.x: Real-Time

#~/ti-linux-kernel-dev/
git checkout origin/ti-linux-rt-4.14.y -b tmp

Build:

#~/ti-linux-kernel-dev/
./build_kernel.sh

Root File System

Debian 9

User Password
debian temppwd
root root

Download:

#~/
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-9.5-minimal-armhf-2018-07-30.tar.xz

Verify:

#~/
sha256sum debian-9.5-minimal-armhf-2018-07-30.tar.xz
85a89cdf8aa40cd757cce4a5519a80dc805f9c354855fc37f01d8dd899149f7d  debian-9.5-minimal-armhf-2018-07-30.tar.xz

Extract:

#~/
tar xf debian-9.5-minimal-armhf-2018-07-30.tar.xz

Ubuntu 18.04 LTS

User Password
ubuntu temppwd

Download:

#~/
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/ubuntu-18.04.1-minimal-armhf-2018-07-30.tar.xz

Verify:

#~/
sha256sum ubuntu-18.04.1-minimal-armhf-2018-07-30.tar.xz
2e401950d75cbf5a6250b8c29a0fbf935f31c49c5373daca77d15903fdbcdb3c  ubuntu-18.04.1-minimal-armhf-2018-07-30.tar.xz

Extract:

#~/
tar xf ubuntu-18.04.1-minimal-armhf-2018-07-30.tar.xz

Setup microSD card

For these instruction we are assuming, DISK=/dev/mmcblk0, lsblk is very useful for determining the device id.

export DISK=/dev/mmcblk0

Erase partition table/labels on microSD card:

sudo dd if=/dev/zero of=${DISK} bs=1M count=10

Install Bootloader:

#~/
sudo dd if=./u-boot/MLO of=${DISK} count=1 seek=1 bs=128k
sudo dd if=./u-boot/u-boot.img of=${DISK} count=2 seek=1 bs=384k

Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.

sudo sfdisk --version
sfdisk from util-linux 2.27.1
#sfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
4M,,L,*
__EOF__
#sfdisk <= 2.25.x
sudo sfdisk --unit M ${DISK} <<-__EOF__
4,,L,*
__EOF__

Format Partition:

for: DISK=/dev/mmcblk0
sudo mkfs.ext4 -L rootfs ${DISK}p1
 
for: DISK=/dev/sdX
sudo mkfs.ext4 -L rootfs ${DISK}1

Mount Partition:
On most systems these partitions may will be auto-mounted…

sudo mkdir -p /media/rootfs/
 
for: DISK=/dev/mmcblk0
sudo mount ${DISK}p1 /media/rootfs/
 
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/rootfs/

Install Kernel and Root File System

To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.

-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=4.X.Y-Z]
-----------------------------

Copy and paste that “export kernel_version=4.X.Y-Z” exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.

export kernel_version=4.X.Y-Z

Copy Root File System

#~/
sudo tar xfvp ./*-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/

Set uname_r in /boot/uEnv.txt

#~/
sudo sh -c "echo 'uname_r=${kernel_version}' >> /media/rootfs/boot/uEnv.txt"

Copy Kernel Image

Kernel Image:

#~/
sudo cp -v ./ti-linux-kernel-dev/deploy/${kernel_version}.zImage /media/rootfs/boot/vmlinuz-${kernel_version}

Copy Kernel Device Tree Binaries

#~/
sudo mkdir -p /media/rootfs/boot/dtbs/${kernel_version}/
sudo tar xfv ./ti-linux-kernel-dev/deploy/${kernel_version}-dtbs.tar.gz -C /media/rootfs/boot/dtbs/${kernel_version}/

Copy Kernel Modules

#~/
sudo tar xfv ./ti-linux-kernel-dev/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/

File Systems Table (/etc/fstab)

sudo sh -c "echo '/dev/mmcblk0p1  /  auto  errors=remount-ro  0  1' >> /media/rootfs/etc/fstab"

Click Boards

U-Boot can currently load up to 4 overlays thru /boot/uEnv.txt To load an overlay, remove the # and replace the fileX with the matching name. ```bash #uboot_overlay_addr0=/lib/firmware/.dtbo #uboot_overlay_addr1=/lib/firmware/.dtbo #uboot_overlay_addr2=/lib/firmware/.dtbo #uboot_overlay_addr3=/lib/firmware/.dtbo ```

ETH CLICK

  • bb-cape-overlays: (minimum version: 4.4.20170927.0-0rcnee1)
  • Kernel: (minimum version: 4.4/4.9/4.14)
#ETH CLICK
PB-SPI0-ETH-CLICK.dtbo
PB-SPI1-ETH-CLICK.dtbo

ETH WIZ CLICK

  • bb-cape-overlays: (minimum version: 4.4.20171005.0-0rcnee1)
  • Kernel: (minimum version: 4.4.91-ti-r133/4.9.53-ti-r67/4.14.0-rc3-ti-r2)
#ETH WIZ CLICK
PB-SPI0-ETH-WIZ-CLICK.dtbo
PB-SPI1-ETH-WIZ-CLICK.dtbo

RTC CLICK

  • bb-cape-overlays: (minimum version: 4.4.20170928.1-0rcnee1)
  • Kernel: (minimum version: 4.4/4.9/4.14)
#RTC CLICK
PB-I2C1-RTC-CLICK.dtbo
PB-I2C2-RTC-CLICK.dtbo

RTC 5 CLICK

  • bb-cape-overlays: (minimum version: 4.4.20171002.0-0rcnee1)
  • Kernel: (minimum version: 4.4/4.9/4.14)
#RTC 5 CLICK
PB-SPI0-RTC-5-CLICK.dtbo
PB-SPI1-RTC-5-CLICK.dtbo

RTC 6 CLICK

  • bb-cape-overlays: (minimum version: 4.4.20170927.0-0rcnee1)
  • Kernel: (minimum version: 4.4/4.9/4.14)
#RTC 6 CLICK
PB-I2C1-RTC-6-CLICK.dtbo
PB-I2C2-RTC-6-CLICK.dtbo

MPU 9DOF CLICK

  • bb-cape-overlays: (minimum version: 4.4.20171004.0-0rcnee1)
  • Kernel: (minimum version: 4.14.0-rc3-ti-r1)
#MPU 9DOF CLICK
PB-I2C1-MPU-9DOF-CLICK.dtbo
PB-I2C2-MPU-9DOF-CLICK.dtbo

WEATHER CLICK

  • bb-cape-overlays: (minimum version: 4.4.20171004.1-0rcnee1)
  • Kernel: (minimum version: 4.4/4.9/4.14)
#WEATHER CLICK
PB-I2C1-WEATHER-CLICK.dtbo
PB-I2C2-WEATHER-CLICK.dtbo

THUNDER CLICK

  • bb-cape-overlays: (minimum version: 4.4.20171004.2-0rcnee1)
  • Kernel: (minimum version: 4.4/4.9/4.14)
#THUNDER CLICK
PB-I2C0-THUNDER-CLICK.dtbo
PB-I2C1-THUNDER-CLICK.dtbo

Remove microSD/SD card

sync
sudo umount /media/rootfs