# POE Power options for Tycon RPPL1224-36-35

**URL:** <https://forum.digikey.com/t/poe-power-options-for-tycon-rppl1224-36-35/28825>\
**Category:** Power\
**Tags:** tycon-systems-inc, power, line-protection-distribution-backups\
**Created:** [February 20, 2023, 2:52pm UTC](https://forum.digikey.com/t/poe-power-options-for-tycon-rppl1224-36-35/28825 "2023-02-20T14:52:48Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![thefixitguybms](https://avatars.discourse-cdn.com/v4/letter/t/46a35a/32.png) [@thefixitguybms](https://forum.digikey.com/u/thefixitguybms)\
**Post date:** [February 20, 2023, 2:52pm UTC](https://forum.digikey.com/t/poe-power-options-for-tycon-rppl1224-36-35/28825/1 "2023-02-20T14:52:48Z")

</div>

I working on a system for WIFI. The system uses POE injection. Receiver is 24v with max of 7 watts 0.3 amps max and Transmitter is 48v 9 watts 0.5 amps max. If Im reading correctly it seems as though the Tycon RPPL1224-36-35 offers POE power of 24v or 48 v. Is there a way that I could supply both without the addition of the added power consumption of an inverter and POE injectors? this is my first build with solar to power these units so I need advice please.

---

<div class="post-metadata">

**Author:** ![Kristof\_2649](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/kristof_2649/32/2325_2.png) [@Kristof\_2649](https://forum.digikey.com/u/Kristof_2649)\
**Post date:** [February 20, 2023, 3:32pm UTC](https://forum.digikey.com/t/poe-power-options-for-tycon-rppl1224-36-35/28825/2 "2023-02-20T15:32:25Z")

</div>

Thank you for your inquiry.

I know the datasheet says 24V at 1.2A _and_ 48V at 0.62A but if you scroll down to system ordering they offer two different part numbers, one for 24V POE output and another for 48V POE output.

 ![image](https://global.discourse-cdn.com/digikey/original/3X/3/f/3f9a43bf035c6f6b471dbeda7de54681c533b105.png)