# Qualification Is the Foundation of Reliable Resistor Selection

**URL:** <https://forum.digikey.com/t/qualification-is-the-foundation-of-reliable-resistor-selection/70614>\
**Category:** Resistors\
**Tags:** tech-tips, part-identification\
**Created:** [July 17, 2026, 6:50pm UTC](https://forum.digikey.com/t/qualification-is-the-foundation-of-reliable-resistor-selection/70614 "2026-07-17T18:50:12Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![TT\_Electronics](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/tt_electronics/32/69101_2.png) [@TT\_Electronics](https://forum.digikey.com/u/TT_Electronics)\
**Post date:** [July 17, 2026, 6:50pm UTC](https://forum.digikey.com/t/qualification-is-the-foundation-of-reliable-resistor-selection/70614/1 "2026-07-17T18:50:12Z")

</div>

Selecting resistors for aerospace and defence electronics often includes reviewing the applicable qualification requirements at an early stage. For component engineers, however, that is rarely where the evaluation ends.

Qualification reports provide the evidence that a resistor design has successfully completed the recognised electrical, mechanical and environmental testing. Qualification evidence provides an important assessment of the design and manufacturing process against defined requirements. Engineers may still need to examine ongoing process controls, lot acceptance, change management and application-specific performance when assessing long-term programme suitability.

As platform lifecycles continue to increase and supply chains evolve, engineers are increasingly evaluating not only whether a resistor has been qualified, but also how it is manufactured, how it performs under application-specific conditions and how effectively the supplier can support the programme over the long term.

Qualification demonstrates capability. Ongoing production demonstrates repeatability.

## **What Happens After Qualification?**

Standards such as MIL-PRF-55342, IEC 60115 and ESCC are fundamental to component selection, providing recognised methods for evaluating environmental endurance, mechanical integrity and electrical stability. Typical qualification programmes include load-life endurance, temperature cycling, moisture resistance, vibration, mechanical shock and short-time overload. Key electrical parameters such as resistance and temperature coefficient of resistance (TCR) are verified before and after testing.

For component engineers, these results establish confidence that the resistor design is suitable for its intended application. A key next step is determining whether that level of performance can be consistently reproduced throughout production.

Material selection, substrate quality, thick-film deposition, firing profiles, laser trimming and passivation all influence long-term electrical stability. Equally important are the manufacturing controls behind those processes. Statistical process control (SPC), lot traceability and disciplined engineering change management help ensure production devices continue to perform consistently with the original qualified design. At TT Electronics, more than 40 years of manufacturing experience, supported by millions of component-hours of load-life testing, provides valuable engineering evidence to support long-term reliability assessments and the FIT estimates used during system reliability modelling.

For programmes expected to remain in service for twenty years or more, this depth of manufacturing knowledge is every bit as important as successful qualification.

## **The Application Matters**

Qualification testing evaluates components under a defined set of controlled stresses. Operational environments are rarely so predictable.

A resistor specified for an aircraft flight control computer is exposed to different electrical loading and environmental conditions than one used in a radar power supply, electronic warfare system or satellite communications subsystem. Understanding those conditions helps determine which qualification data deserves the closest scrutiny.

Beyond the qualification report, engineers should consider:

- Load-life stability and resistance drift
- Resistance shift following thermal cycling
- Temperature coefficient of resistance (TCR) across the operating range
- Resistance stability following humidity exposure
- Surge and overload performance where applicable
- Mechanical integrity following vibration and assembly stresses
- Long-term product availability and controlled engineering changes

Taken together, these considerations help engineers interpret qualification data in the context of the intended operating environment.

## **Completing the Engineering Assessment**

Completing the engineering assessment means understanding not only how a resistor performed during qualification, but how consistently that performance can be maintained throughout the life of the programme. Controlled manufacturing processes, disciplined engineering change management, production traceability and long-term product support all contribute to reducing both technical and supply chain risk.

Considering these factors alongside recognised qualification data provides a more complete picture of resistor suitability for demanding aerospace and defence applications.

## **Applying These Principles**

These broader considerations are also relevant when evaluating the [TT Electronics Welwyn CR Series of thick-film chip resistors](https://www.digikey.com/en/products/detail/wec/CR0805F-10RFI/29353133?s=N4IgjCBcoLQdIDGUBmBDANgZwKYBoQB7KAbRAE4AOAVhAF0BfBggJlJAGEAlehoA).

Manufactured in Bedlington, United Kingdom, the CR Series uses established thick-film technology and is available across multiple package sizes, resistance values and tolerance options. The range is approved to applicable EN 140401 and CECC 40401 specifications and supports analogue, control, power-management and signal-conditioning functions in aerospace, defence and other long-life electronic applications.

Electrical ratings and qualification status remain central to the selection process, but they should be considered alongside the intended operating conditions and the manufacturing and programme controls available for the selected part. Depending on the application, these may include lot traceability, configuration control, change notification and continued product support.

Qualification therefore provides an important foundation for resistor selection. Combining that evidence with application-specific analysis and an understanding of the supplier’s manufacturing and lifecycle controls helps engineers make more complete component decisions for long-term programmes.