RE: PICO-PI-IMX7 and Siging In/Um?


#58

Hello Sir,

I am out of space. I think I know where I left off. Is the u-boot cli cmd control-c and reset out of place on the wiki?

Seth

P.S. I tried things and I cannot get enough space for now to put in new directories w/ info.


#59

Sir,

I am reinstalling Ubuntu on my machine. I am going way back.

Seth

P.S. After the new install, I will revisit all these ideas and boot the PICO board.


#60

Hello Sir,

I cannot load the DFU agent in the u-boot cli so I can load the SPL binaries at /u-boot/.

Load the SPL binary via dfu-util:

**~/u-boot**

`sudo dfu-util -D SPL -a spl`

Seth

P.S. Do you have any recommendations on this effort? dfu in u-boot is busted and I cannot move on from that point. I will research some more.


#61

@silver2row, why can’t you load the dfu agent in u-boot? Please show the error you are getting…

Regards,


#62
=> dfu 0 mmc 0
Couldn't find part #1 on mmc device #0
DFU entities configuration failed!
(partition table does not match dfu_alt_info?)
dfu - Device Firmware Upgrade

Usage:
dfu <USB_controller> <interface> <dev> [list]
  - device firmware upgrade via <USB_controller>
    on device <dev>, attached to interface
    <interface>
    [list] - list available alt settings

@RobertCNelson

Hello,

This is the issue. I think I may have read your jumper pin incorrectly for the PICO board jumpers. I thought the header pins were switched around in the photo. I did not know the header pins were situated where they were in the photo for eMMC Boot Mode. I got the USB Boot Mode done correctly. There was not a way to goof that one up.

Seth

Here is the terminal issue when attempting a DFU command:

torx@forket:~/u-boot$ sudo dfu-util -D SPL -a spl
dfu-util 0.9

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/

dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
dfu-util: No DFU capable USB device available

I can interpret what I did earlier if that makes any difference. I know exactly what happened now, i.e. incorrect jumper positions.


#63

DFU needs a partition “table” to operate… Let’s create one as a temp, just to get things loaded…

First run on the Pico:

ums 0 mmc 0

Next, on your development machine: (replace DISK with /dev/sdX, look at lsblk and use the new driver that’s the pico…)

sudo dd if=/dev/zero of=${DISK} bs=1M count=10

sudo sfdisk ${DISK} <<-__EOF__
1M,,L,*
__EOF__

sudo mkfs.ext4 -L rootfs ${DISK}1

Now in u-boot kill the “ums 0 mmc 0” and rerun the “dfu 0 mmc 0”…

Regards,


#64

Yes Sir,

Thank you for replying. @RobertCNelson: It worked like a charm.

Seth

P.S. You have been more than patient. I appreciate the support.


#65

@RobertCNelson,

Okay sir, at the end of the instruction set, when you type out reset in the u-boot cli, what should I do w/ u-boot once it resets?

Seth

P.S. I am asking b/c the board disappears from the desktop and I pushed the button before three seconds was over when u-boot booted back in the u-boot cli. Please send guidance.


#66

@silver2row, well if you followed the full directions after calling “reset” it should boot into linux. Please show what u-boot is dumping to the serial console.

Regards,


#67

Sir,

** No partition table - mmc 0 **
switch to partitions #0, OK
mmc0(part 0) is current device
** Unrecognized filesystem type **
starting USB...
USB0:   Port not available.
USB1:   USB EHCI 1.00
scanning bus 1 for devices... 1 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found

Device 0: device type unknown
... is now current device
BOOTP broadcast 1
BOOTP broadcast 2
DHCP client bound to address 192.168.1.10 (1565 ms)
*** ERROR: `serverip' not set
Cannot autoload with TFTPGET
missing environment variable: pxeuuid
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/01-00-1f-7b-86-a1-b0
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C0A8010A
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C0A8010
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C0A801
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C0A80
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C0A8
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C0A
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C0
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/C
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/default-arm-mx7
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/default-arm
*** ERROR: `serverip' not set
missing environment variable: bootfile
Retrieving file: pxelinux.cfg/default
*** ERROR: `serverip' not set
Config file not found
BOOTP broadcast 1
DHCP client bound to address 192.168.1.xx (96 ms)
*** ERROR: `serverip' not set
Cannot autoload with TFTPGET
BOOTP broadcast 1
DHCP client bound to address 192.168.1.xx (182 ms)
*** ERROR: `serverip' not set
Cannot autoload with TFTPGET

Seth

P.S. This is what happens once I try to let u-boot’s reset option go past the three second mark. I will try again. Do I need tftpget and do I need to use /dev/ttyUSB1 instead?


#69

@silver2row

** No partition table - mmc 0 **
switch to partitions #0, OK
mmc0(part 0) is current device
** Unrecognized filesystem type **
starting USB...

This just means you need to go back and run (from U-Boot console):

ums 0 mmc 0

Then on your development desktop, mount the new usb drive that shows up and follow this section of the wiki…

https://www.digikey.com/eewiki/display/linuxonarm/PICO-PI-IMX7#PICO-PI-IMX7-SetupmicroSDcard

Regards,


#70

Sir,

Should I go through that section only or through that section and until the end of the instruction set?

Seth

P.S. I have tried just about everything. I am not questioning you b/c you do not know things about adding boards via CC and u-boot but I want to make sure I get it right this time. This way, if something arose b/c of my actions dedicated to the board configuration, I could post again to get better help.


#71

Hello Sir,

Here is the u-boot dump.

=> reset
resetting …

U-Boot SPL 2019.01-rc3 (Jan 12 2019 - 18:11:15 -0600)
Trying to boot from MMC1

U-Boot 2019.01-rc3 (Jan 12 2019 - 18:11:15 -0600)

CPU: Freescale i.MX7D rev1.2 1000 MHz (running at 792 MHz)
CPU: Commercial temperature grade (0C to 95C) at 36C
Reset cause: POR
Board: i.MX7D PICOSOM
I2C: ready
DRAM: 512 MiB
PMIC: PFUZE3000 DEV_ID=0x30 REV_ID=0x11
MMC: FSL_SDHC: 0
Loading Environment from MMC… OK
In: serial
Out: serial
Err: serial
Net: FEC0
Hit any key to stop autoboot: 0
Saving Environment to MMC… Writing to MMC(0)… OK
** No partition table - mmc 0 **
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1…
Found /boot/extlinux/extlinux.conf
Retrieving file: /boot/extlinux/extlinux.conf
189 bytes read in 104 ms (1000 Bytes/s)
1: Linux 4.20.1-armv7-lpae-x2.1
Retrieving file: /boot/vmlinuz-4.20.1-armv7-lpae-x2.1
** File not found /boot/vmlinuz-4.20.1-armv7-lpae-x2.1 **
Skipping Linux 4.20.1-armv7-lpae-x2.1 for failure retrieving kernel
SCRIPT FAILED: continuing…
starting USB…
USB0: Port not available.
USB1: USB EHCI 1.00
scanning bus 1 for devices… 1 USB Device(s) found
scanning usb for storage devices… 0 Storage Device(s) found

Device 0: device type unknown
… is now current device
FEC0 Waiting for PHY auto negotiation to complete… TIMEOUT !
Could not initialize PHY FEC0
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
BOOTP broadcast 12
BOOTP broadcast 13
BOOTP broadcast 14
BOOTP broadcast 15
BOOTP broadcast 16
BOOTP broadcast 17

Retry time exceeded; starting again
missing environment variable: pxeuuid
Retrieving file: /boot/extlinux/pxelinux.cfg/01-00-1f-7b-86-a1-b0
FEC0 Waiting for PHY auto negotiation to complete… TIMEOUT !
Could not initialize PHY FEC0
*** ERROR: serverip' not set Retrieving file: /boot/extlinux/pxelinux.cfg/00000000 FEC0 Waiting for PHY auto negotiation to complete......... TIMEOUT ! Could not initialize PHY FEC0 *** ERROR:serverip’ not set
Retrieving file: /boot/extlinux/pxelinux.cfg/0000000
FEC0 Waiting for PHY auto negotiation to complete… TIMEOUT !
Could not initialize PHY FEC0
*** ERROR: serverip' not set Retrieving file: /boot/extlinux/pxelinux.cfg/000000 FEC0 Waiting for PHY auto negotiation to complete......... TIMEOUT ! Could not initialize PHY FEC0 *** ERROR:serverip’ not set
Retrieving file: /boot/extlinux/pxelinux.cfg/00000
FEC0 Waiting for PHY auto negotiation to complete… TIMEOUT !
Could not initialize PHY FEC0
*** ERROR: serverip' not set Retrieving file: /boot/extlinux/pxelinux.cfg/0000 FEC0 Waiting for PHY auto negotiation to complete......... TIMEOUT ! Could not initialize PHY FEC0 *** ERROR:serverip’ not set
Retrieving file: /boot/extlinux/pxelinux.cfg/000
FEC0 Waiting for PHY auto negotiation to complete… TIMEOUT !
Could not initialize PHY FEC0
*** ERROR: serverip' not set Retrieving file: /boot/extlinux/pxelinux.cfg/00 FEC0 Waiting for PHY auto negotiation to complete......... TIMEOUT ! Could not initialize PHY FEC0 *** ERROR:serverip’ not set
Retrieving file: /boot/extlinux/pxelinux.cfg/0
FEC0 Waiting for PHY auto negotiation to complete… TIMEOUT !
Could not initialize PHY FEC0
*** ERROR: serverip' not set Retrieving file: /boot/extlinux/pxelinux.cfg/default-arm-mx7 FEC0 Waiting for PHY auto negotiation to complete... done *** ERROR:serverip’ not set
Retrieving file: /boot/extlinux/pxelinux.cfg/default-arm
*** ERROR: serverip' not set Retrieving file: /boot/extlinux/pxelinux.cfg/default *** ERROR:serverip’ not set
Config file not found
BOOTP broadcast 1
BOOTP broadcast 2
DHCP client bound to address 192.168.1.xx (1997 ms)
*** ERROR: serverip' not set Cannot autoload with TFTPGET BOOTP broadcast 1 DHCP client bound to address 192.168.1.xx (207 ms) *** ERROR:serverip’ not set
Cannot autoload with TFTPGET

At one point, I was thinking this was going to work w/out the Ethernet cable. I tried to plug in the Ethernet cable and as you can see, the same info. popped up.

Sir, do I need to umount or sync the device at all once I follow the instructions?

I still cannot sign in via ssh, too. Now, I have a rootfs system on my desktop even when my board is not plugged in. Does this make any sense to you?

Seth


#72

@silver2row

Found /boot/extlinux/extlinux.conf
Retrieving file: /boot/extlinux/extlinux.conf
189 bytes read in 104 ms (1000 Bytes/s)
1: Linux 4.20.1-armv7-lpae-x2.1
Retrieving file: /boot/vmlinuz-4.20.1-armv7-lpae-x2.1
** File not found /boot/vmlinuz-4.20.1-armv7-lpae-x2.1 **
Skipping Linux 4.20.1-armv7-lpae-x2.1 for failure retrieving kernel
SCRIPT FAILED: continuing…

You are getting closer, it looks like you didn’t correctly copy the kernel image/rootfs… From this section:

https://www.digikey.com/eewiki/display/linuxonarm/PICO-PI-IMX7#PICO-PI-IMX7-CopyKernelImage

Regards,


#73

Sir,

When I am in USB Boot Mode, I receive this complaint: Header Tag is not an IMX imagee)�.

Does this mean anything?

Seth

P.S. I will attempt to try again.


#74

You have no reason to go back to USB Boot Mode, at this point just leave it in eMMC Boot mode running “ums 0 mmc 0” and correctly copy the kernel files…

Regards,


#77

@RobertCNelson,

Sir…Seth here. I am still trying here. Um, The u-boot cli is stuck on:

=> reset
resetting ...

I figured it is b/c of the dfu 0 mmc 0 command in u-boot. I tried to use it and then I went to my dev. desktop to put in the sudo dfu-util -D SPL -a spl command. I was unable to do so again. Now, when I listen to the instructions you gave me for,

    sudo dd if=/dev/zero of=${DISK} bs=1M count=10
    sudo sfdisk /dev/sdb <<-__EOF__
    1M,,L,*
    __EOF__

    sudo mkfs.ext4 -L rootfs /dev/sdb1

I get an error.

Seth

P.S. The error is the same as above, i.e.

torx@forket:~/u-boot$ sudo dfu-util -D SPL -a spl
dfu-util 0.9

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/

dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
dfu-util: No DFU capable USB device available

#78

@silver2row, What does U-Boot console show?

Regards,


#79
=> ums 0 mmc 0
UMS: LUN 0, dev 0, hwpart 0, sector 0x0, count 0x720000
CTRL+C - Operation aborted
=> reset
resetting ...

Right now, this is what u-boot console shows. While the cmd dfu 0 mmc 0 is typed and after I press enter, nothing.

It just makes me think that I need to use the cmd in the development desktop.

Seth


#80

@silver2row, you only need to use run “dfu 0 mmc 0” once, it’s mostly about updating the ancient default bootloader (while in USB Boot Mode) to mainline U-Boot, so we can boot in eMMC Boot mode with a U-Boot that has a good version of “ums 0 mmc 0”…

At this point you have a good version of U-Boot in the eMMC, just mount the drive with “ums 0 mmc 0” and write the rootfs to the drive.

Regards,