why?
No, can you get to u-boot prompt?
Regards,
why?
No, can you get to u-boot prompt?
Regards,
Yes Sir,
I can get to u-boot in USB Boot Mode.
Seth
P.S. Oh and sir, the reason I used sdb0 was b/c of this line in the instructions, " Example: for DISK=/dev/mmcblkX, when X was 0 in the old instruction log. I just thought I could exchange X (0) from mmcblk0 to sdb0. That is the answer. My fault. I know now.
Okay, do this again:
First run on the Pico:
ums 0 mmc 0
Next, on your development machine: (replace DISK with /dev/sdX, look at lsblk and use the new driver that’s the pico…)
sudo dd if=/dev/zero of=${DISK} bs=1M count=10
sudo sfdisk ${DISK} <<-__EOF__
1M,,L,*
__EOF__
sudo mkfs.ext4 -L rootfs ${DISK}1
Now in u-boot kill the “ums 0 mmc 0” and rerun the “dfu 0 mmc 0”…
The “/dev/mmcblkX” node is special when compare to a normal block device…
Normal Block devices go: /dev/sda → /dev/sdb → /dev/sdc, with partitions starting with “1, 2, 3…”
Where as the “/dev/mmcblkX” devices goes: /dev/mmcblk0 → /dev/mmcblk1 → /dev/mmcblk2 with partitions starting, p1, p2, p3…
Regards,
Sir,
sudo sfdisk ${DISK} <<-__EOF__
> 1m,,L,*
> __EOF__
Checking that no-one is using this disk right now ... FAILED
This disk is currently in use - repartitioning is probably a bad idea.
Umount all file systems, and swapoff all swap partitions on this disk.
Use the --no-reread flag to suppress this check.
sfdisk: Use the --force flag to overrule all checks.
Seth
P.S. This is when I run: sudo sfdisk ${DISK} <<-EOF and I have gotten this error before. I tried things I know but I have failed so far.
No sir,
I have not done that yet. I will get on it.
Seth
Sir,
Do I need to build the Linux Kernel every time I make errors w/ the instructions or is it there for future use, as is?
Seth
P.S. I removed automount in my Ubuntu Desktop. I guess I will restart the machine and see if it took place.
Sir,
Well, I have a new error:
Checking that no-one is using this disk right now ... OK
Disk /dev/sdb: 539.5 KiB, 552448 bytes, 1079 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
>>> Created a new DOS disklabel with disk identifier 0xd5747866.
/dev/sdb1: Start sector 2048 out of range.
Failed to add #1 partition: Numerical result out of range
Leaving.
…
This is w/ the cmd in the dev. desktop: sudo sfdisk ${DISK} <<-__EOF__
Seth
P.S. I am moving on from here and trying more items. If you come up w/ any ideas, please contact me when you have some time.
Disk /dev/sdb: 539.5 KiB, 552448 bytes, 1079 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
So the “eMMC” on your PICO is now 539.5KiB in size…
umount the drive
sudo umount /dev/sdb
Fully unplug the PICO…
and delete the invalid device node…
sudo rm -rf /dev/sdb
and start again… It sounds like you dd’ed SPL/u-boot.img before you mounted the eMMC…
Regards,
Yes Sir,
I tried to set up from scratch again. I am getting an error at dfu 0 mmc 0 in the u-boot console.
Seth
P.S. Here it is: I know we walked through this before. I erased/removed the /dev/sdb dir. and tried to umount the board but umount stated that the board was not mounted.
=> dfu 0 mmc 0
Couldn’t find part #1 on mmc device #0
DFU entities configuration failed!
(partition table does not match dfu_alt_info?)
dfu - Device Firmware Upgrade
Usage:
dfu <USB_controller> [list]
dfu 0 mmc 0
Couldn’t find part #1 on mmc device #0
DFU entities configuration failed!
DFU needs a valid partition, so do this again…
First run on the Pico:
ums 0 mmc 0
Next, on your development machine: (replace DISK with /dev/sdX, look at lsblk and use the new driver that’s the pico…)
sudo dd if=/dev/zero of=${DISK} bs=1M count=10
sudo sfdisk ${DISK} <<-__EOF__
1M,,L,*
__EOF__
sudo mkfs.ext4 -L rootfs ${DISK}1
Regards,
Sir,
Should I perform the u-boot cmd ums 0 mmc 0 and then the commands below in your instructions and then try to sudo umount /dev/sdb and then sudo rm -rf /dev/sdb?
Seth
It depends… If sfdisk reports the disk to be too small again, then yes…
Regards,
Yes Sir,
Thank you…@RobertCNelson: Here is the command umount /dev/sdb on the dev. desktop terminal.
sudo umount /dev/sdb
umount: /dev/sdb: not mounted.
Seth
P.S. I have been reading on umount in the man pages. Should I load lazily, i.e. -l? I am sure you can tell, this is my first rodeo. Anyway, Where, if at any point, should I start on the instructions after I cannot umount my device?
@silver2row, in u-boot type:
ums 0 mmc 0
Then on your PC, type:
sudo fdisk -l /dev/sdb | grep ^/dev
and report what you get…
Regards,
sudo fdisk -1 /dev/sdb | grep ^/dev
fdisk: invalid option -- '1'
Try 'fdisk --help' for more information.
Sir, I think I just narrowed down the issue. Would it be -l (el) instead of -1 (one)? If not, that is using the -1 in the command you told me to use and stated in the above terminal printout.
Seth
That was an “-l” as in list…
Ps: you can copy n paste from the browser.
Regards,
Sir,
I think this is where I went wrong in the instructions: sudo sfdisk ${DISK} <<-__EOF__
! After this command, I typed in 1M (as in one emm). Now, I think I may have had to type in or copy, lM (el emm). Am I right?
Seth
P.S. Here is the list from fdisk:
sudo fdisk -l /dev/sdb | grep ^/dev
/dev/sdb1 * 2048 7471103 7469056 3.6G 83 Linux
Those l’s look like 1’s. Sorry.
In the case of “1M” for sfdisk, that’s “one Megabyte”… not “L Megabyte”…
Based on your last post, you are right here after “ums 0 mmc 0”
SERIAL_CONSOLE_U_BOOT
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
Net: FEC0
Hit any key to stop autoboot: 0
=> ums 0 mmc 0
So go to here, and “copy n paste” the commands directly, don’t “try” to type them yourself…
Regards,
Sir,
This is in u-boot: ums 0 mmc 0.
This is my print out on the dev. desktop after the first command in the last link you gave when in /u-boot and typing: sudo ~/imx_usb_loader/imx_usb SPL
sudo ~/imx_usb_loader/imx_usb SPL
config file </home/torx/imx_usb_loader//imx_usb.conf>
vid=0x066f pid=0x3780 file_name=mx23_usb_work.conf
vid=0x15a2 pid=0x004f file_name=mx28_usb_work.conf
vid=0x15a2 pid=0x0052 file_name=mx50_usb_work.conf
vid=0x15a2 pid=0x0054 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0061 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0063 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0071 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x007d file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0080 file_name=mx6ull_usb_work.conf
vid=0x1fc9 pid=0x0128 file_name=mx6_usb_work.conf
vid=0x15a2 pid=0x0076 file_name=mx7_usb_work.conf
vid=0x1fc9 pid=0x0126 file_name=mx7ulp_usb_work.conf
vid=0x15a2 pid=0x0041 file_name=mx51_usb_work.conf
vid=0x15a2 pid=0x004e file_name=mx53_usb_work.conf
vid=0x15a2 pid=0x006a file_name=vybrid_usb_work.conf
vid=0x066f pid=0x37ff file_name=linux_gadget.conf
vid=0x1b67 pid=0x4fff file_name=mx6_usb_sdp_spl.conf
vid=0x0525 pid=0xb4a4 file_name=mx6_usb_sdp_spl.conf
vid=0x1fc9 pid=0x012b file_name=mx8mq_usb_work.conf
no matching USB device found
…
It has always been this way when I try this route. Oh and sir, I see the config file line, line two, states // instead of single /. Does this matter.
Seth