Hi,
The P/N 1877646-4 (KIT, PLUG CONN, GAIN, GPRB2), which we regularly procure, is now listed as Obsolete.
We need to continue procuring this part in higher quantities and repeatedly over an extended period. Therefore, anyone please provide the available alternate or replacement part number for P/N 1877646-4.
Your assistance in identifying a suitable long-term replacement would be greatly appreciated.
This looks to be a highly specialized connector. Our system shows that it went obsolete in 2022. There are no alternatives that I can find for this part.
Thank you, then please suggest if any other similar connector.
The part 1877646-4 was a kit which included all of the parts that were needed less the contacts.
There are options from Radiall USA, but will need to be pieced together.
Here are options for the housings.
Here are the options for the inserts.
Your team will need to evaluate which housing and inserts will work for your application.
Hi, still looking? Does the replacement need to mate with the existing 1877646-4 installation without changes, or could you consider a different connector/interface if it provides a sustainable long-term replacement?
Hello,
Thank you for looking into this issue.
We would prefer an alternate connector that is compatible with the existing P/N 1877646-4 installation. Ideally, the replacement should meet the existing installation requirements, or require only minor modifications to the existing installation to accommodate the different connector.