Standard Flow, Reverse Flow, & Reversible Air Flow Fans

There are two sides to a fan when referencing airflow, the Impeller side and the Strut side.


Impeller Side which is the fan blade side.
image


Strut Side which holds the fan motor and label.
image


Both Standard Flow and Reverse Flow fans blow air in only one specified (but opposite) direction where Reversible Flow fans are capable of moving air in either direction. Each having their own advantages whether using them for intake or exhaust, and what side you need the motor on depending if you want the motor to run cooler or warmer.

Standard fans pull air from the Impeller side and blow air out of the Strut side, sometimes called impeller intake fans:

image


Reverse Air Flow Fans pull air from the Strut side, and blow air out of the Impeller side, sometimes called strut intake fans:
image


Although less common, Reversible Air Flow fans are capable of blowing air in either directions:


How Reversible Fans are Controlled

Previously, if the designer wanted to achieve two different directions of airflow, two fans would be required. This arrangement added cost to the bill of materials (BOM), required more room in the design to accommodate both fans, increased maintenance requirements, and lowered product reliability as two fans could be a point of failure. A single fan with directional and speed control capability had been highly desirable to overcome these flaws of the two-fan design. In recent years reversible flow fans have been engineered to meet these needs. PWM speed control is a method where a fixed frequency AC square wave signal is provided to the fan and the Duty Cycle of the waveform is altered to match the desired speed, as shown below.
image

The frequency is typically fixed at 25Khz, but most manufacturers accept a range of frequencies as specified on their data sheets. By varying the duration of time the waveform is positive voltage (HIGH) versus zero volts (LOW), the speed of the fan is controlled varying from 0% to 100%. This 0% duty cycle to 100% duty cycle can be matched to the fan speed curve in any fashion desired. But typically a customer will want a 0% duty cycle to represent a completely stopped or minimal RPM fan, with 100% representing full speed operation. It is important to note that 0% duty cycle is the same as grounding the PWM control wire (0 V), and 100% duty cycle is the same as holding the line at a positive voltage HIGH state. Many manufacturers also design fans so that a disconnected “Floating” PWM input line will run the fan at 100% RPM, similar to a non-PWM controlled fan, allowing for flexibility in different applications. Reversible fans extend this control paradigm by segmenting the PWM duty cycle curve into “Forward” versus “Reverse” regions, as shown in the graphic below.

This segmentation still allows for speed control over a condensed duty cycle range, while creating a system whereby the direction of flow can be controlled without requiring additional control wires or circuitry. In most cases a simple firmware or software change in the customer’s equipment can create the capability of controlling the direction, with minimal disruption of industry standard control assumptions. A generous “stop” region is provided in the duty cycle curve to ensure the fan is at 0 RPM when required.

Reversible Flow Applications

Reversible flow fans are a specialty design that enables some unique use cases. It should be noted however that the performance of these fans is asymmetrical. The forward flow performance will always differ from the reverse flow performance due to differences in how the blades are optimized and the aerodynamics of the venturi as it affects air flow. This means that the forward airflow CFM and static pressure will differ from the reverse flow specifications. The amount of variation differs depending on the frame size and design, but these differences should be listed in the product data sheet. Despite this limitation, there are some cases where Reversible Flow is the perfect solution to unique problems. Some examples of these are:

  • Fans used in outdoor applications where the device normally intakes air in one direction, but a periodic reverse flow helps to ensure that air pathways do not become clogged with bugs or other environmental debris. This can reduce costly maintenance visits to remote locations.
  • Fans used in equipment where seasonal environmental changes create the need for different airflow of intaking versus exhausting air.
  • Situations where a “confidence check” is needed to confirm the proper operation of air flow monitoring sensors.
  • Applications where dynamic control of air flow pathways is needed, and large air flow check valves may be difficult or impossible to integrate.
  • HVAC applications where occasional intake of environmental air is required to comply with building codes.

Other applications include vending machines, cooler display cases, and lighting. In nearly all cases, reversible flow functionality can also be combined with other features such as Tachometer and Alarm monitoring for a comprehensive control suite.


See Also:
Source - Orion - Reversible Flow Fans Paper
Click here for all DigiKey Fans and Fan Accessories
How to select a Fan Type (Axial, Centrifugal and Blower)
Fan Selection & Application Guide
What makes a Fan noisy
Fan Types
Orion Fan Wire Color Codes and Special Functions