Schneider Modicon M221 Programmable Logic Controller

M221 at a Glance

The Schneider Electric M221 is a family of Nano PLCs made to control basic automation for machines. The PLC is programmed using [EcoStruxure Machine Expert Basic software] (https://www.se.com/us/en/download/document/MachineExpertBasicV1_4/). The hardware is expandable using TM3 expansion modules.

  • At the time of this writing, DigiKey offered 28 unique models:

    • The lowest cost unit is the TM221C16T featuring 16 points (nine inputs and seven semiconductor outputs).
    • One of the largest is the TM221CE40U featuring 40 points (24 inputs and 16 semiconductor outputs).
  • Individual family members vary in terms of:

    • Output ports with options for both relay and semiconductor
    • Power supply with options for 24 VDC or AC units supporting 100 ~ 240VAC
    • The number and type of serial and Ethernet ports
    • The number allowable expansion modules physically attached to the side of the PLC

There are other differences that can be discovered by reviewing DigiKey’s parametric search engine for the Modicon M221 PLC.


This article is part of the DigiKey Field Guide for Industrial Automation

Location: Select It → PLCs
Difficulty: :gear: Engineer — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 03 Aug 2026


Comparing the M221 to Other Modicon Models

The M221 family is a mid-tier PLC within the extended Schneider lineup.

Figure 2: Family hierarchy of Schneider PLCs.

M221 Accessories

The M221 PLC is designed for expansion using a variety of modules that clip to the right side of the PLC.

  • The TMH2GDB HMI as shown in Figure 1 is a natural extension for the M221.

  • DigiKey has nearly 60 expansion modules including:

    • Digital input and output
    • Analog input and output
    • Temperature (thermocouple)
  • A variety of plug-in cartridges are available for the M221. These modules are installed on the face of the PLC. An example is the TMC2AI2 input and the TMC2AQ2C output module. These allow the PCL to interface with 4-20 mA sensors and actuators.

  • DigiKey offers safety modules

  • DigiKey also offers the TM3XTRA1 transmitter and TM3XREC1 receiver pair. When connected with an RJ45 cable, the modules add simple remote I/O capabilities to the M221 family. This is a unique configuration as the remote I/O uses the same expansion modules as the PLC. For example, a TM3AI2HG module could be attached directly to the M221 PLC while another TM3AI2HG is attached to the TM3XREC1.

Tech Tip: There are thousands of combinations and permutations for the Modicon M221. Recommend you use the Schneider PLC configurator to plan out your M221 configuration. An example configuration is shown in Figure 3 featuring the remote expansion modules.

Figure 3: Screen capture from the Schneider M211 PLC configuration tool showing the RJ45-connected remote modules.

Related Components

The Schneider M221 PLC provides the logic and control of a machine or industrial process. It is never installed in isolation. DigiKey has a growing number of supporting products. This list contains related Schneider Electric products:

  • Motor starters and motor starter accessories. A small but important piece is the LUFC00. As shown in Figure 4, the PLC to motor starter wiring effort is reduced to a single RJ45 connection.

  • Power supplies such as the 24 VDC ABLM1A24025 or the larger three-phase input ABLU3A24200.

Figure 4: M221 with simplified connection to a motor starter.

Material from DigiKey’s Workbench

These DigiKey-generated TechForum articles authored by DigiKey Application Engineer Aaron Dahlen feature the M221 PLC:

Frequently Asked Questions

How do I program the M221?

The Modicon M221 is programmed using Schneider’s EcoStruxure Machine Expert software.

  • Connection is made via a USB cable.

  • The PLC is programmed in several different IEC 61131-3 languages including:

    • Ladder Diagram (LD)
    • Instruction List (IL)
    • Grafcet (Sequential Function Chart (SFC))

This article shows an example program featuring a LD User Defined Function Block (UDFB) as shown in this screen capture.

What is meant by Book and Brick Style?

The terms book and brick (standard) describe the M221 PLC’s form factor. The difference is seen in Figure 2:

  • Book style describes a PLC that is more upright - like a book. It consumes less DIN rail space when compared to its counterpart. Note that the I/O connections are closely spaced in the lower right-hand side of the PLC.

  • Brick (standard) style describes a conventional looking PLC. The PLC is designed with the inputs on the top and outputs on the bottom.

Can the M221 PLC be expanded?

Yes, there are multiple ways to expand the M221 PLC’s functionality including:

  • Plug-in cartridge installed on the face of the PLC
  • Expansion module that are installed to the right of the PLC
  • TM3XTRA1 transmitter and TM3XREC1 receiver remote I/O
  • Select models feature an Ethernet port enabling connection to a wide variety of Modbus equipped devices.

:books: Continue Exploring Industrial Control Systems

If this discussion was helpful, you may also want to explore:

:world_map: DigiKey Navigation

About This Author

Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.

Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.

Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.