------Question for 7100320463 Please Put your question below------
What is the SCOTCH-WELDEPOXY ADHESIVE DP125 suitable gun and syringe?
------Question for 7100320463 Please Put your question below------
What is the SCOTCH-WELDEPOXY ADHESIVE DP125 suitable gun and syringe?
@raj.bharath Welcome to DigiKey’s TechForum!
It has 3 different Duo-Pak type, 48.5ml, 200ml and 400ml, and they use different applicators and nozzles.
This brochure will help to identify which applicator and nozzle will suit for each dup-pack size.
For example, if you are going to use 7100320278 which is 48.5ml Duo-Pak, then you have to use 3M157692-ND applicator and 3M157629-ND (or 3M157693-ND) nozzle.
Best regards,
Hi Brain Lee,
We purchased the below item. I already ordered the applicator and nozzles. Please provide the suitable applicator and nozzles.
Hello @raj.bharath,
As you can see from the product detail page, it is 48.5ml Duo-Pak.
So, you can use the recommended applicator and nozzle above.
Best regards,
Hi Brain Lee,
Yes its 48.5ml Duo-Pak. My I know the below I ordered is suitable to the DP 125 48.5ml Due-Pak?
@raj.bharath,
8DG-50-1-1-ND is MG Chemicals’ applicator, and as it is from different manufacturer we cannot confirm if it is compatible with 3M’s Duo-Pak (Even they both are based on Mixpac DMA and support 50ml 1:1 cartridge, we have no information if they are compatible or not).
As you have already placed an order, you can check it yourself after receiving it.
Best regards,
Hi Brain Lee,
Due to my urgency already placed the order.