Siemens ET200 SP Distributed IO Checklist

This is a checklist used to restore connectivity between the Siemens PLC and the ET 200SP.


This article is part of the DigiKey Field Guide for Industrial Automation

Location: Program It → Distributed I/O
Difficulty: :gear: Engineer — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 06 Mar 2026


Device Configuration

  • Verify the TIA Portal configuration matches the real-world devices. Pay attention to version:

    • Version of the ET 200SP Interface module.

    • Version of the Server Module. Don’t make my mistake and assign V1.2 when the actual version is V1.12. In this case, the base V1.1 is required by TIA Portal.

    • Version of each of the submodule(s).

Power

Network Connectivity

  • Use the ping command to verify basic network functionality for both the PLC and ET 200 SP.

TIA Portal Configuration

  • Apply the PROFINET device name e.g., io device_1. I’ve included Figure 1 as a reminder as I often forget this step and then wonder why the system diagnostics displays the hardware component not available message.

  • Verify that the TIA Portal configuration matches the real-world port use (e.g., X1 vs X2).

  • Set the partner port (“ANY port” vs PLC specific).

  • Compile and the download the hardware and software.

Figure 1: PROFINET name screen.

Troubleshoot using the PLC’s Diagnostic Data

Figure 2 presents the PLC diagnostics screen for. As part of the troubleshooting process, it is sometimes useful to power cycle the PLC. In this example we see:

  • 12:18:11: Supply voltage missing
  • 12:18:20: Reboot
  • 12:18:28: Hard fault from an AS-i networked device


Figure 2: Diagnostics screen for the PLC.

About This Author

Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.

Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.

Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.