Sikwal Mini – A Compact and Professional RP2350 Development Board

:small_blue_diamond: Project Overview

Sikwal Mini is a compact development board built around the Raspberry Pi RP2350 (QFN-60) microcontroller.
The board is fully designed by Sikwal with the goal of creating a:

Small

Clean

Easy-to-use

Production-ready

Professional RP2350 platform

It is optimized for daily prototyping, sensor projects, audio modules, and embedded systems.


:small_blue_diamond: Bottom Layer (Routing Layer)

The first image shows the bottom layer of the PCB:

Fine-pitch routing coming out of the QFN-60 package

Clean fan-out with no crossing conflicts

Well-organized trace flow from the MCU to the GPIO pin headers

Large GND pour (dark purple) for signal stability

Balanced routing on the left and right sides

Rearranged tracks to reduce noise and improve signal integrity

The layout clearly demonstrates a strong understanding of QFN routing, especially considering the number of pins and the small board size.


:small_blue_diamond: Top Layer (Components Layer)

The second image shows the top layer where all main components are placed:

Key Components Visible:

U2 – RP2350 microcontroller (center of the board)

X2 – 12 MHz crystal oscillator placed very close to XIN/XOUT

C1, C2 – 22 pF crystal load capacitors

U1 – Voltage regulator (3.3V)

C20–C25 – 10 µF and 1 µF decoupling capacitors

SW1 – Reset button

L3 – 2.2 µH inductor for the RP2350 power section

D1, D2 – USB protection / power diodes

Right & left pin headers for GPIO expansion

H2 – SWD 1×4 programming header

U4 – USB-C port footprint at the bottom

The top layout is organized, with short traces and correct placement for power and crystal stability.


:small_blue_diamond: Design Strengths

:check_mark: Excellent Component Placement

MCU in the center → Power → Crystal → I/O around the edges.
This is exactly how a professional microcontroller board should be structured.

:check_mark: Proper USB-C Integration

The USB connector is positioned at the bottom for easy access and enclosure design.

:check_mark: Crystal Layout Done Correctly

Very short trace length

Symmetrical routing

Load capacitors placed next to the crystal

This ensures stable 12 MHz operation.

:check_mark: Clean GPIO Header Arrangement

Pin headers on both sides make the board breadboard-friendly and easy to prototype with.

:check_mark: Ready for PCB Assembly

All components are SMD, correctly oriented, and placed with enough spacing for automated pick-and-place machines.


:small_blue_diamond: Purpose of the Project

The Sikwal Mini board was created to:

Practice and master QFN-60 routing

Build a small but complete RP2350 platform

Prepare for batch manufacturing and assembly

Support future audio and studio-analysis projects

Serve as a smaller version before the larger Project Al-Waraqah RP2350


:small_blue_diamond: Current Status

PCB design completed

Component placement finalized

Routing optimized and clean

Board is now ready for manufacturing

Next Steps

Generate BOM + Pick-and-Place

Order first batch (20 assembled pieces)

Perform initial power-up and GPIO testing

Publish open-source files

Prepare for eBay listing


:small_blue_diamond: Summary

Sikwal Mini shows a high-level PCB design skill, with professional routing, clean organization, and correct electrical placement.
It is a solid, production-ready RP2350 development board designed entirely by Sikwal.