Hi,
I’m trying to get voice call audio over USB on a SIM7600G-H (firmware LE20B01SIM7600G-M11_OTA) and I’m stuck. Calls connect fine, and the module accepts the audio configuration from SIMCom’s USB AUDIO application note: AT+CPCMREG=1 returns OK, CPCMFRM 0 and 1 return OK, and CUSBAUDIO, CODECCTL and CSDVC are all accepted. But no PCM ever moves on interface 4, in either direction.
On the Linux tty the host writes about 80 KB of 8 kHz/16-bit PCM per call and only the first couple of frames go in, then it blocks with EAGAIN. Downlink is always 0 bytes. Same story with a raw usbfs claim on interface 4: bulk OUT times out and bulk IN never returns anything. I’ve tried 8 kHz and 16 kHz, enabling PCM at dial, after answer and during ringing, both AT ports, module resets and re-plugs, and USB 2 and USB 3 passthrough. The serial AT ports and the USB descriptors are all fine.
Has anyone actually got USB PCM audio streaming on this module? Is there a firmware requirement I’m missing, e.g. does this build not run the PCM engine at all?
Happy to share logs if useful. Thanks.