Smd code KLe datasheet help me pls
This is a difficult question.
We need to know the exact dimensions of this element.
SOT-323 2mmx2.1mm size
Hello berk_2,
Thank you for the information, unfortunately, I have been able to find anything related to that marking.
Are you able to provide more information related to the board it is mounted on? Is there any marking on the board that may assist in identifying this?
yes this send me pic same 2.1mm - 2.3mm including feet
What function does this board perform?
Can you take a big photo with the surrounding components?
Do you know the structure of this component (N-P-N, P-N-P, Mosfet)?
Or is it a microchip?
Would you happen to have a sharper image, one with out the markings on it?
Again:
What function does this board perform (model)?
Do you know the structure of this component (N-P-N, P-N-P, Mosfet)?
Could you draw which pin is which for Gate Drain Source? It’s hard to make out.
We have similar MOSFets like TSM2N7002AKCU but I wouldn’t recommend it until the pinout is verified.
This 2sk3018 sot 323 smd code KN but not understand
Most likely it’s a transistor MCH3411.
KL - MCH3411.pdf (47,1 КБ)
Thank you so much
You are Welcome.![]()