We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
The top marking looks like a United Chemi-Con logo. The value would be 100uf at 6.3 volts. I have linked a data sheet for that manufacture that shows the top marking. You would need to measure the footprint to get the correct case size.
Our TRANE non-programmable thermostat stopped working… After pulling off the cover this cap just fell out. Might be the issue
We’re a little confused on the markings. Its a surface mount capacitor. Our guess is its 6.5 uF and the 50k is the tolerance? Sorry just trying to figure this thing out and where to buy. Thanks for your help
I am trying to verify the markings on this cap however, it is more likely the 100 is calling out the 100uF and the 50 is 50 volts and the k is 10% this would leave the 655 being a series marking or date code.
I think Robert’s interpretation is likely quite good. The 100uF/50V SMT caps we’ve got in stock can be found here.
Check for leads on the bottom-if they’re still there, it may have just been a bad solder joint. If that’s the case, you might be able to simply solder the thing back into place. On the other hand, there’s a fair chance that if parts are falling off the unit, that there’s more than just this issue gone amok.
Ttank you both for the reply! Unfortunately it looks like one lead broke off so we will just order on digikey and see if it fixes the problem. Hopefully if someone else runs into this issue with the same thermostat they now have a solution.
Hello - this is part of a LED headlight / turn signal controller. It seems that capacitor failure is common and identifying a source for them would help a lot of car guys. The circled one is most common and I have a board that has one connector broken off the board. Is a replacement available from Digikey?
Thank you very much - I’ll pass this information on to a young man who is an up & coming board-level whiz. However, I started to place an order for this item and it reports as back ordered. Is there any other compatible item that is in stock?
Hi, I am hoping to identify a capacitor which has been giving me trouble for quite some time. It is from an LG Flatron monitor which, after many years of faithful service, began to make a loud whining noise as it turned on, eventually morphing into flashing off and on several times until it stabilized, and eventually into continually flashing and never fully turning on. I suspect, from the loud whining noise and the flashing, that it’s a capacitor, and from what I can see of the circuit board, it only has 2, one being tiny and the other being quite large. I suspect the large one has seen its last day, but it doesn’t look completely burst, and for the life of me I can’t figure out how to read the code on it to identify what kind of capacitor I’ll need in order to replace it. I assume “100v” means 100 volts, but from what I’ve seen of other capacitors, even that may not be an accurate assumption. I’ve been stuck using my old 720p monitor for a couple of years now, and I would love to get my primary back in service.
Hello Robbie. Thank you very much for contacting us, and I hope what I found helps.
I recognized the logo on that capacitor as being for the Samyoung company. I’ve been looking through their catalog for surface mounted capacitors, and I do believe that the marking shown does call out 33µF 100V.
The ones I could find where the top line (the lot code) ends in a J are the BXJ series, rated up to 105°C. In that series, the 33µF 100V is called out as being 10mm diameter, 10mm height, and a 10.3mm*10.3mm surface mount land size. The closest match I could find in our stock to that capacitance, voltage, size, and temperature is the Nichicon UUX2A330MNL1GS, Digi-Key 493-6281-1-ND.
Fantastic! That looks to be the same size! I wasn’t sure with what I had been reading whether the 33 meant 33µF or 3.3µF, since those were both available options and I honestly am not well-versed enough in electronics to know which would be normal for a monitor. I was lost researching it at first, too, because I thought the first symbol was a weirdly misshapen 6. It wasn’t until I started looking at other capacitors online that I realized it’s some kind of company logo instead. xD
Hi Welcome to techforum! the one marked 560 would be a 56uf and 4 should be the voltage. I am unable to verify the size by photos, but you can check link below for part UWX0G560MCL1GB to see if would work after you measure you part. This one is 0.209"" L x 0.209"" W (5.30mm x 5.30mm) in size. The other looks like 680 which would be 68uf ( confirm the 6, as it also might be a 5?, photo is a little distorted on that number.) You can check out 732-8471-1-ND for that one, it is a 6.8v, we do not have anything in a 4V for that one. Again, depending on your dimensions. This one is 0.209"" L x 0.209"" W (5.30mm x 5.30mm)
Glenda