Stripping PUR Cable Without Nicking the Conductor Insulation

Industrial automation control cables are often manufactured with a polyurethane (PUR) jacket. The cables are robust, yet this durability makes cable prep challenging. This engineering brief demonstrates a method of removing the jacket without nicking the conductor’s insulation using the tool shown in Figure 1.

Featured Products

The featured products are shown in Figure 2.


This article is part of the DigiKey Field Guide for Industrial Automation

Location: Teach It → Shop Practices
Learning Pathway: Industrial Automation Technician → Industrial Sensors
Difficulty: :seedling: Student — difficulty levels explained
Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 02 Nov 2026


Figure 1: PUR-jacketed cable inserted into a stripping tool.

Figure 2: PUR-jacketed M12 cable alongside the tools used to strip the flying leads.

Configuring the Weidmüller CST tool

The CST tool contains multiple blades. The depth of each blade may be set individually using the setscrews shown in Figure 3. In this brief we only require one blade to remove the cable’s PUR jacket. Close inspection of Figure 1 shows that the center blade is engaged, while the blade on the left has effectively been remove due to the setscrew setting.

The cutting depth is set based on the pass/fail criterion described in the pass/fail section.

Figure 3: Setscrews used to adjust blade cutting depth.

Jacket Separation

The secret is to score the jacket as shown in Figure 4. Score the jacket without cutting all the way through as this will keep the blade from touching the conductor’s insulation. With a bit of wiggling and bending, the PUR jacket will tear at the score mark. Stated another way, it will take some effort to pull off the scored jacket section, but it should not require additional hand tools or a second pass from the cutting tool.

Figure 4: The jacket is scored without being cut through.

Pass or Fail Condition

The final step is to examine the individual wires as shown in Figure 5. Verify that the blade has not nicked the insulation. This is best done by gently folding back the wires and looking for damage at the base where the wires extend from the jacket.

Observations for the featured tools:

  • There is a balance between score depth and the ability to tear the jacket. Too deep and the conductors insulation is nicked. Too shallow and you will damage the the cable by bending and twisting it in an attempt to tear the jacket. A 1/4 turn can make the difference between acceptance and rejection using this Weidmüller tool.

  • There are slight variations in cable jacket diameter. This is a normal part of the manufacturing process. However, it can make a difference with the cutting depth. Recommend each new cable be stripped and inspected before committing to the real work. This also catches wildly inappropriate cutter settings left over from the last job. There is a good argument for purchasing a tool for each type of cable. Did I mention that community toolboxes and precision tool settings do not go together? As a thought experiment, compare the cost of setup time and wasted materials against the cost of dedicated tools.

  • Discipline is required when spinning the tool around the cable. Make one turn, and one turn only about the cable. This discipline is necessary as the blade is apt to dig deeper on subsequent passes thereby damaging the conductor’s insulation.

Tech Tip: If the wire insulation is nicked, you failed.

Period.

Cut the end off and start again.

As a guiding principle, industrial control systems have a lifecycle measured in decades. A small error or carelessly overlooked detail is a gremlin in the machine. Never forget that a single downtime event can wipe away any cost savings from skipping the cable rework.

Figure 5: Final inspection of the conductors.

About This Author

Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.

Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.

Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.