Susumu resistor kit resistor values?

------Question for RG2012PB-KIT-FILE Please Put your question below------

What resistor values are in the Susumu resistor kits, in particular the RG2012PB-KIT-FILE which seems to have 120 values from 47 ohms to 1 megaohm?

There are 105 possible E24 series values in this range, and quite a bit more than 120 values of E96. And, which of these resistors are 0.5% and which 0.1% as all values should exist in the 0.1% range.

And, just to check: the lower precision kit RG2012PD-KIT-FILE has full E24 series from 10 ohms to 1 megaohm (120 values), and the higher precision kit RG2012NW-KIT-FILE has full E24 series from 47 ohms to 470 kiloohms (97 values).

Hello lmk and welcome to the DigiKey TechForum.

If you scroll down to the bottom of the product page, each of these kits lists the part number and quantity of the resistors included, example below.

Thanks. This shows a part of kit contents, but even with “show more” selected, I only see first 20 lines of the 120 resistors included in the kit (which do not further seem to be in any particular order, neither alphabetical for component name or SKU no by their resistor values).

Though, this indeed suggest that the kit has some resistor values duplicated in 0.1% and 0.5% tolerance (like 1M), so this could at least explain the non-expected count of different resistor values for the RG2012PB kit. The other two kits based on the 20 shown lines could indeed be full E24 series collections (as all shown resistor SKU are the E24 series values and there does not seem to be any duplicates unlike with the RG2012PB kit).

I noticed that the product pages have been updated to include the full list of resistor values. Thanks! This solved my question.

1 Like