Switch application

R1966ABLKBLKESGRN

The circuit this switch will operate in is 12vDc

Will the LED light up at this voltage?

Welcome to the Technical Forum . The illumination voltage listed under the product attributes is 2.2 volts. The drawing on the website lists 2 volts to a max of 2.6 volts.

Hi @mwt ,

EG5448-ND is an alternative 12V illuminated option.

Click here for comparison link EG5448-ND | EG1859-ND as there are some differences such as lower current handling and termination to mention a few. Otherwise a properly calculated resistor can be used with original switch on the 12V source.