# Ta vs TC vs Tj Ratings

**URL:** <https://forum.digikey.com/t/ta-vs-tc-vs-tj-ratings/762>\
**Category:** Digikey.com Navigation and Terminology\
**Tags:** faqs, terminology\
**Created:** [November 23, 2017, 12:00am UTC](https://forum.digikey.com/t/ta-vs-tc-vs-tj-ratings/762 "2017-11-23T00:00:20Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![Robert\_Fay](https://sea2.discourse-cdn.com/digikey/user_avatar/forum.digikey.com/robert_fay/32/6529_2.png) [@Robert\_Fay](https://forum.digikey.com/u/Robert_Fay)\
**Post date:** [November 23, 2017, 12:00am UTC](https://forum.digikey.com/t/ta-vs-tc-vs-tj-ratings/762/1 "2017-11-23T00:00:20Z")

</div>

Many of our semiconductor products have ratings that are dependent on temperature. you many see something like Current-Continuous Drain (Id) @25°C and it shows a rating of 30mA(Tc) or 30mA(Tj) or 30mA(Ta). Often time customer does not understand what these ratings mean. It gets even more confusing when manufactures list a rating similar to part BSZ034N04LSATMA1TR-ND which has a Current - Continuous Drain (Id) @ 25°C rating of 19A (Ta), 40A (Tc).

Here is a brief summary of these ratings:

Ta = Ambient temperature. This is a still air temperature reading for the environment that the semiconductor is in.  
Tc = Case temperature. This is the temperature reading of the case of the semiconductor device.

> Ta would normally mean the environment is cooled and kept at 25°C whereas Tc would mean the device is forcibly cooled through a directly attached heatsink and cooled to the 25°C.

Tj = Operating Junction temperature. This is the temperature of the device circuit itself under given conditions. Tj must be calculated from the Tc and/or Ta.  
TJmax = Maximum Junction temperature. This is the maximum temperature that the device tolerate.